2024-02-18 9:20 PM - last edited on 2024-02-18 11:57 PM by KDJEM.1
this is the same issue as previously reported in a thread that had an answer marked as a solution (it was not, in fact, a solution)
I am looking to test X-CUBE-EEPROM on a supported eval board. (nucleo-G431RB)
I load the relevant X-CUBE-EEPROM project into my workspace "existing projects into workspace option"
I can see all the files and when I go to compile it "succeeds" but with 4 warnings that there are no implementations for _close_r, _lseek_r, _read_r, and _write_r
when I go to run my firmware on the target board it doesn't work (as you'd probably expect)
When I load other target projects from the same package up in STM32 cube IDE I get the same errors when I go to build.
I am running STM32 cube IDE 1.14.1 and AFAIK this install is auto-updating, I don't see any updates I am missing)
the ide works fine for other projects (like the one I am actually developing, as well as an example project for a sensor I used recently to test that with an eval board before doing it in my project) but this X-CUBE-EEPROM example seems completely dead, at least if I want to use STM32 cube IDE?
.
2024-02-19 6:06 AM
@Julian1 wrote:I can see all the files and when I go to compile it "succeeds" but with 4 warnings that there are no implementations for _close_r, _lseek_r, _read_r, and _write_r
See: https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904
@Julian1 wrote:when I go to run my firmware on the target board it doesn't work (as you'd probably expect)
Those are just warnings - so shouldn't necessarily stop the code from working.
You need to give more details of what, exactly, is "not working"
Use the debugger to see what's going on ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.