cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-CELLULAR on B-U585-IOT02A Hard faults when executing AT+CGMR handler. The SID_CTXT.device_info pointer is NULL when memcpy is called to copy the response into the struct. On L4, the pointer is NULL also but the code continues.

MSher.1
Associate III

at_modem_signalling.c fRspAnalyze_CGMR() line 1583. In L4 the compiler is v5, on U5 the compiler is v6. It seems the main issue is that the device_info pointer is not initialized before this code executes. CS_get_device_info() is called later after CS_power_on().

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.