2024-01-22 2:00 AM
In LwIP examples for NUCLEO-H723ZG, in the linker, I think that there is an incorrect range of RAM_D2 memory.
For example here:
MEMORY
{
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ROM (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
}SRAM available from 0x30000000 has 32 kB available
from the reference manual:
Or am I missing something? I am writing here before creating an issue on GitHub as I am not sure I am not misreading something. I think they took it from the STM32H74x/H75x devices as those have this amount of memory.
The example works correctly as the addresses used are hard-coded in the application, but the size should be correct either way.
Solved! Go to Solution.
2024-01-22 4:24 AM
Hello @heveskar ,
Thank you for reporting this issue.
I confirm the typo , it is a known issue and it is already reported internally.
Internal ticket number: 152716 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity :).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 3:04 AM
You are correct, the RAM size of SRAM1 & SRAM2 in D2 is 16kB each.
There are many errors in many ST files, probably the typical copy & paste.
BTW, in the H723 - H735 series, ethernet DMA can access AXI RAM, although use of descriptors (and maybe some RX/TX buffers if space allows) in D2 = SRAM1 & SRAM2 is preferred, as the ethernet MAC also resides in D2. (See block diagram RM0468, page 107)
2024-01-22 4:24 AM
Hello @heveskar ,
Thank you for reporting this issue.
I confirm the typo , it is a known issue and it is already reported internally.
Internal ticket number: 152716 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity :).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 4:33 AM
Thanks.
2024-03-18 1:31 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.