2023-05-21 7:20 AM
The logic in functions HAL_SAI_Abort() and HAL_SAI_DMAStop() is flawed because the sequence of actions is wrong. A proper sequence is:
In the current implementation the function SAI_Disable() is called after stopping the DMA. This causes a SAI underrun and a data glitch at the end of stream. The bug seems to be present for all series with SAI peripheral.
Also the two functions do almost the same and the code is also almost the same, which is an example of a bad and bloated design.
Solved! Go to Solution.
2023-05-31 3:26 AM
Transmitting/receiving anything other (including the silence) than the intended data creates a glitch. And in general an underrun/overrun is an abnormal situation, not something that is acceptable to happen almost always.
The particular issue is not even close to being complex and the fact, that the HAL team cannot understand such a simple issue even when pointed to it, just proves again what I'm saying all the time - the level of incompetence is just absolutely tragic.
2023-05-28 11:33 AM
Hello @Piranha,
It seems Data glitch cannot happen with the current HAL_SAI implementation. Because the SAI sends a MUTE value (0x00) in case of underrun.
I will escalate this internally for deep check.
Thanks
Imen
2023-05-31 3:26 AM
Transmitting/receiving anything other (including the silence) than the intended data creates a glitch. And in general an underrun/overrun is an abnormal situation, not something that is acceptable to happen almost always.
The particular issue is not even close to being complex and the fact, that the HAL team cannot understand such a simple issue even when pointed to it, just proves again what I'm saying all the time - the level of incompetence is just absolutely tragic.
2023-06-05 6:55 AM
Hello @Piranha,
I confirm the first issue and it is reported internally.
Internal ticket number: 152756 (This is an internal tracking number and is not accessible or usable by customers).
With regards
Omar
2023-10-09 10:33 PM
Hello @Piranha ,
I just checked my code and found that I'm not using HAL, but copied the sequence from HAL:
I never got an underrun error (or so I think...), I can't really say anything about glitches, because I never listen to SAI data, just checking it visually in our scope / FFT app.
When I switched the order of disables (as you suggest) I didn't see any difference.
Question:
I would prefer to have the currently used DMA buffer filled completely, but right now I'm not sure how to get there cleanly.
Maybe via transfer complete interrupt, set flag there, check flag elsewhere, then stop sequence?
2024-03-18 1:32 AM - edited 2024-03-18 1:34 AM
Hello All,
I would inform you that this issue is fixed in the new release of STM32CubeF4 (v1.28.0).
The HAL SAI has been updated to improve audio quality (avoid potential glitch).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.