2021-11-20 6:02 AM
Hello,
I am working on Nucleo-h745ziq board. According the Ux_Device_CDC_ accordingly I create project for Nucleo-H745ziq board. After connecting the user USB to port I have to go device driver and update the port after that I get the port in Tera term and after it takes time for connecting why this happen ? And when I transmit data over the UART port data is not get received on USB port why? I set the baud rate 115200.Can u help me?
2021-12-14 6:01 AM
Hello @MDeva.1 ,
You can refer to the following example
Try to port it on your board. This may help you.
BeST Regards,
Walid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.