2016-12-06 12:50 AM
This is my first microcontroller besides an HCS12 I used in class, and I am a little confused. I have updated the firmware to the latest version, and have used mbed to do a blink LED and test the GPIO. However, this is all done from pre-built functions. Where can I find the library for the Nucleo STM32F303K8 board to create my own programs? Thanks in advanced.
#beginner #stm32 #nucleo #library #stm32f3 #stm32_usb_device_library2016-12-06 1:13 AM
Hi
deepshah93
,You can create you own project using the STM32CubeF3 library wich can be dowloaded from this
. For STM32F303K8-Nucelo go to this path STM32Cube_FW_F3_V1.6.0\Projects\STM32F303K8-Nucleo . Check the ready-to-use example there and start you own project by using the template project.-Walid F-
2016-12-06 10:54 PM
Thank you! This may sound silly, but to put this project onto the MCU, do I just put the main.c, main.h, and related files into the MCU from Windows Explorer? Mbed generates a .bin file and I was not sure if I upload the files generated from STM32Cube into mbed so they can be compiled into a .bin file.
2016-12-07 1:49 AM
Hi
deepshah93
,For mbed project, I recommend that youuse the mbed compiler at this
https://developer.mbed.org/handbook/mbed-Compiler
which allow you to import the Cube library.-Walid F-
2016-12-13 5:27 PM
I am able to create new projects using mbed with importing the stm32f30x.h library, but I still do not know how to import the Cube library that I create. I tried to import it and received many errors.
2016-12-13 5:43 PM
I used the modified Eclipse program and saw when I build the application there is a .bin file in the debug folder, is this what I will be transferring to the MCU?
2016-12-14 3:43 AM
you would follow relevant handbook guide lines n the mbed web site ->
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.