2021-02-05 1:00 AM
Hi all,
This post is obviously coming from a person without any USB development experience.
We use some off-the-shelf instruments which I know to be based on STM32, and they connect to a PC using the Virtual COMPort. Nothing new here, the standard Windows drivers perfectly recognizes it and I can communicate using any console program.
What we would like to do is to get rid of the PC: make an external "controller" device with another STM32 with USB OTG to which the instrument would be connected (a small LCD and a few buttons will be the interface to whatever the instrument requires). Our controller would recognize the VCP, and "convert it back" to a serial transport layer.
So I guess we are looking for the C/C++ "reverse" of the VCP driver.
[STM32_INSTRUMENT]-------->(USB_CABLE)-------->[STM32_USB_OTG][SERIAL_DATA]
Does anyone know if there is such a thing available?
Thanks,
Bruno
Solved! Go to Solution.
2021-02-09 10:16 AM
ie a HOST not a DEVICE
STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone
2021-02-09 8:10 AM
Just touching this again to see if anyone can come up with any ideas?
What do I need to be able to read serial data in a STM32 that arrives via USB, where on the other end we have another STM32 using Virtual COMPort?
Thanks!
2021-02-09 10:16 AM
ie a HOST not a DEVICE
STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone
2021-02-10 1:16 AM
Hello TDL, thank you for the reply.
As I mentioned, my question was obviously written by someone with no USB experience! ;)
Your answer does show the right path, thanks again. For those looking for more info, now that I've learned the proper term, a Google search for "stm32 cdc_standalone" points to some interesting material.
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.