STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CUBE_FW_L5_V1.3.1 does not exist.

I want to start an example project for the STM32L562E-DK Developer Kit.After I 've selected any example for this MCU I always get the error messageDOWNLOAD of 'STM32Cube_FW_L5_V1.3.1' FAILEDHow can I solve this? Or How can I install a patch?br

AGeis.1 by Associate
  • 933 Views
  • 1 replies
  • 0 kudos

Where to route the external ETH PHY interrupt signal, so it would be used as sub-interrupt in the MAC peripheral?

The part I am using it the STM32H753II. Trying to use the MAC peripheral I got stuck at PYH interrupt, for which is stated to be included as one of the sub-interrupts of the module (last bullet of 58.8.3). The corresponding mask and status bits are w...

BMače.1 by Associate
  • 720 Views
  • 0 replies
  • 0 kudos

Resolved! application jump to system memory bootloader

Hi,I have an stm32l43 connected as a USB device. Using the BOOT0 pin, I can start the built-in Bootloader and use DFU. Now I wish to jump to the BL without this Pin by a software jump.But with this jump, I only seem to reset the device (my code start...

Audio data RF synchronization

Hello,I am sampling audio data with sampling rate 16 kHz and then send it using RF to the other MCU which is sending to DAC samples with the same 16 kHz sampling rate, Im using DMA for sending data through I2S to external DAC. The problem is that the...

KD�?b by Associate II
  • 810 Views
  • 0 replies
  • 0 kudos

STM32F746-Discovery Kit Audio Player

Hi, ​​I have gone through below link. ​​https://community.st.com/s/question/0D50X0000AIcIc6SQF/audio-player-demo-stm32l4r9idisco?t=1604201466282​Is there any demo for audio player from that audio files pop up from USB Mass Storage/SDCard in TouchGFX...

Wrong pinout configuration with LL_GPIO_Init()

 GPIO_InitStruct.Pin = I2C1_SCL_Pin|I2C1_SDA_Pin; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN; LL_GPIO_Init(GPIOB, &GPIO_InitStruct);Code above ...

AVoro.19 by Associate
  • 1432 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.