2022-01-06 2:03 AM
Hello,
I wanted to use the CORTEX_M4F_STM32F407ZG-SK demo of free rtos with stm32f401cc. In the past I have used this demo with stm32f405rg, I have changed the PLL setting for 84Mhz as:
// in stm32f4xx.h
#define HSE_VALUE ((uint32_t)25000000)
// in system_stm32fxx.c
/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */
#define PLL_M 25
#define PLL_N 336
/* SYSCLK = PLL_VCO / PLL_P */
#define PLL_P 4
/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */
#define PLL_Q 7
I am using IAR(and changed the mcu to stm32f401cc), but when I run the code, it jumps directly to the HardFault_Handler without going through main. I am using FreeRTOSv202104.00 version.
2022-01-06 2:59 AM
Check SystemInit() code.
Make sure it enables FPU.
Look at what instructions fault, the CPU has registers.
Use the debugger to step in from Reset_Handler, it unchecked "run to main()" type options.
Check initial stack pointer is within RAM of MCU
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.