2018-11-20 2:48 AM
I am currently trying to setup lwIP with freeRTOS using CubeMX. Using the generated code, creates a defaultTask, which initilializes the lwIP stack. It works just fine to ping the controller, but what i don't understand is, that in lwipopts.h NO_SYS is set to 1and thus the whole initialization is made for a configuration without RTOS, but it still works.
When i include the sys_arch, also provided by ST(uses the cmsis_os) i get a linker error, which can't find tcpip_try_callback, which is declared in tcpip.h but never defined. Do i have to do that manually or what am i missing here?
Thanks a lot for your help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.