2018-06-20 10:00 AM
Hi all,
I'm using the HAL drivers and STM32CubeMX to generate DMA Burst transfers from memory to TIM1 in OCToggle mode on the Nucleo F722ZE.
Old versions of the HAL drivers had a function called
HAL_StatusTypeDef HAL_TIM_DMABurst_MultiWriteStart(TIM_HandleTypeDef *htim,
uint32_t BurstBaseAddress,
uint32_t BurstRequestSrc,
uint32_t* BurstBuffer,
uint32_t BurstLength,
uint32_t BufferLength)
which is identical to the
HAL_StatusTypeDef HAL_TIM_DMABurst_WriteStart(TIM_HandleTypeDef *htim,
uint32_t BurstBaseAddress,
uint32_t BurstRequestSrc,
uint32_t* BurstBuffer,
uint32_t BurstLength)
except the
BufferLength
#dma #output-compare #hal #dma-burst #burst-mode #toggle #timerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.