2023-03-27 1:26 AM
I generated my code by stm32cubemx,version6.1.2, and use ucpd2 as sink&dead battery,. But got USBPD_ERROR in USBPD_DPM_InitCore after execute " CHECK_PE_FUNCTION_CALL(USBPD_PE_Init(USBPD_PORT_0, (USBPD_SettingsTypeDef *)&DPM_Settings[USBPD_PORT_0], &DPM_Params[USBPD_PORT_0], &dpmCallbacks));
"
Changing stack size is useless;any other solution?
thanks.
Solved! Go to Solution.
2023-03-27 7:03 AM
Hello @LOMO
Are you sure it's not the line above that is generating the error ? I mean the line calling USBPD_CAD_Init.
Can you try to look at the return code of USBPD_CAD_Init ?
I suspect that it could be a memory allocation error, as your Heap in the linker settings seems too low.
You should try to change the heap to 0xC00 and see if that resolves the issue.
Regards
2023-03-27 7:03 AM
Hello @LOMO
Are you sure it's not the line above that is generating the error ? I mean the line calling USBPD_CAD_Init.
Can you try to look at the return code of USBPD_CAD_Init ?
I suspect that it could be a memory allocation error, as your Heap in the linker settings seems too low.
You should try to change the heap to 0xC00 and see if that resolves the issue.
Regards
2023-03-27 6:58 PM
Changing the size of the heap instead of the stack is effective,my problem.thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.