2020-03-27 5:59 AM
Hello, i try to get USB working with the EG91 Modul from Quectel. Is there anywhere a tutorial what steps are to do? Ive read the USB Host Documentation but my device is still in Application idle Mode.
Im using the USB_Host Driver and the CDC Middleware driver.
There are 3 virtual Com Ports in the GSM Modul.
MX_USB_HOST_Init(); and MX_USB_HOST_Process(); are called
2020-03-27 4:48 PM
So you need to implement USB host working with a multi-functional device.
Read the descriptors, find and configure all endpoints for the 3 CDC functions, then drive all needed endpoints (read and write).
Maybe start from driving one function, then add others.
ST does not provide complete example for this; you may want to get a good, commercial USB library, or find a consultant.
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.