2015-05-27 4:31 AM
Hello,
I am using the latest Windows driver from 1.4 package. I am Working on Windows7-64bit. However it tells version 1.3.1. My Project is based on CubeMx USB CDC. My Problem is when I sent a payload with size power_of_2 then the driver does not forward data to PC application. e.g. I sent from uC CDC device 1024 byte - nothing happens in terminal program then I sent 3 bytes from device - then the PC driver delivers the 1024 Byte as well as the 3 Byte to the application. Can anybody confirm this behaviour? Is there any workaound? - probably to split the payload when detected critical size combination. #windows7 #usb #cdc #vcp2015-05-27 6:57 AM
Maybe for some reason the microcontroller doesn't send the NAK packet to inform that there is no more data coming? What USB library are you using?
Also, according to , maximum packet size for USB FS is 1023 bytes, are you using USB FS or USB HS?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.