2021-05-11 6:38 AM
We are using the STM32 USB Device Library.
This is the USB circuit
https://peter-ftp.co.uk/screenshots/20210511523173514.jpg
Does the STM library implement this, or do I need to detect a drop in VBUS (cable to Controller being disconnected), or is no action required?
The concern is that current can flow from those two lines of a powered 32F417 into an unpowered USB Controller. But maybe this doesn't matter.
Many thanks!
2021-06-11 11:43 AM
Can anyone offer any input on this?
There is a 1.5k resistor to +3.3V which is enabled or disabled. This obviously works in normal USB operation where +5V is arriving from the USB Controller, but what if the +5V connection is broken? That is partly what VBUS_SENSE is for - to make sure that resistor is not enabled in that case, because it would feed a bit of current into the controller.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.