cancel
Showing results for 
Search instead for 
Did you mean: 

USB PD library Can't charge Redmi phone

AOhir.1603
Associate III

Hi Yohann,

Created a separate thread as it's a separate issue.

I am having an interesting problem with the latest USB PD library v3.

I configured my board to be a source and connect to my Samsung phone (A20); it works very happily, I can start charging my phone straight away and can do this repeatedly.

However if I connect to another phone (Redmi Note 7), I can't get it to charge the phone. When I was working with the previous version of the library (v2), the redmi phone would start charging without problems.

I've attached a log that shows the difference between v2 and v3.

  • log_charge_redmi_libv2.cpd: trace output for using library v2 and connecting to a redmi phone
  • log_charge_redmi_libv3.cpd: trace output for using library v3 and connecting to a redmi phone

It looks like it sends out the source capability information but for some reason we keep getting a transmission fail alert.

Any idea why it gets a transmission fail alert and how to fix this issue?

Thanks,

AOF

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Yohann M.
ST Employee

Hi AOF,

=> I can only see 1 request from redmi phone (in libv3.cpd trace):

debug 0000018696  P0 DEBUG0  "VbusVolt=4700 "
-pe - 0000018697  P0 PE_SRC_SEND_CAPABILITIES
debug 0000018701  P0 DEBUG0  "VbusVolt=4250 "
--->  0000018702  P0 SOP  s:006 PD3 H:0x11a1 SRC_CAPABILITIES DATA:2c910122
                  OPTION  : DRD DRP
                  FIXED   : voltage 5000mV current 3000mA
 
debug 0000018705  P0 DEBUG0  "ALERT IT1"
debug 0000018706  P0 DEBUG0  "ALERT_TASK"
debug 0000018708  P0 DEBUG0  "Alert=  44    "
debug 0000018710  P0 DEBUG0  "ValidAlert=44 "
<---  0000018711  P0 SOP  s:002     H:0x0001 GOODCRC
<---  0000018713  P0 SOP  s:006 PD2 H:0x1042 REQUEST DATA:2cb10413
                  PDO position          : 1
                  NoUSBSuspend          : 1
                  USB Capable           : 1
                  GiveBack              : 0
                  Capa Mismatch         : 0
                  Operating current     : 3000 mA
                  Maxi Operating current: 3000 mA
                  UnchunkMode Support   : 0
 
-no - 0000018714  P0 NOTIFY_SRCCAP_SENT
debug 0000018715  P0 DEBUG0  "DisableRx"
debug 0000018717  P0 DEBUG0  "Alert= 103    "
-pe - 0000018718  P0 PE_SRC_WAIT_REQUEST
debug 0000018720  P0 DEBUG0  "ValidAlert= 1 "
debug 0000018727  P0 DEBUG0  "CC_S2= 0 "

Quite strange to see a drop of VBUS. Can you confirm that VBUS level is stable with V3 lib? Did you perform this test with your board or EVAL_FUSB board?

Regards,

Yohann

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.