2020-04-20 6:16 PM
Hi there,
I am using the x-cube-usb-pd in TCPM/TCPC configuration (USBPD_TCPM_LIB_PD3_CONFIG_1).
My questions are:
For example, our device has fixed PDO 3A@5V and APDO 3A@6V-12V. If a connected device requests for a Fixed PDO 3A@9V, would it negotiate to provide 3A@9V? Or does a connected device need to have requested for APDO 3A@9V?
For example, our device has Fixed PDO 3A@5V and Variable PDO 3A@6V-12V. A connected device has a Fixed PDO 3A@9V. What happens then?
Thanks,
AOF
2020-04-20 11:04 PM
Hi AOF,
1) Difference between USBPD_TCPM_LIB_PD3_CONFIG_1 and USBPD_TCPM_LIB_PD3_FULL is only the support of VDM. 'CONFIG_1' supports PPS (APDO).
2) Both port partner should have in their capabilities the support of APDO. Sink device can request a APDO if a source devices APDO matches with its capabilities.
In your example, if sink device requests fixed PDO 3A@9V, Source device will reject this request and will stay to default 5V@3A. Sink connected device should request APDO 3A@9V to switch in PPS mode.
3) We did not use variable PDO in our different applications we delivered but I assume that this is the same constraint.
Regards,
Yohann
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.