2025-10-15 3:11 AM
Hello,
I don't seam to see anything related to the implementation of the USB PD AVS system to allow a sink to request voltages of up to 48V. Am I miss-reading the X-CUBE-TCPP code? If it is missing, is there a plan to implement it?
Thanks a lot
Have a nice day
Solved! Go to Solution.
2025-10-15 7:07 AM
AFAIK, you can extend the USB PD stack to parse and handle APDOs (Augmented PDOs) for AVS. Also, X-CUBE-TCPP package already support EPR mode. No hardware platforms for EPR (up to 240W) are provided yet.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-15 7:07 AM
AFAIK, you can extend the USB PD stack to parse and handle APDOs (Augmented PDOs) for AVS. Also, X-CUBE-TCPP package already support EPR mode. No hardware platforms for EPR (up to 240W) are provided yet.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-15 6:11 PM
Oki doki, at least I will not be re-inventing the wheel if I implement that myself. Thanks a lot @FBL
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.