2025-12-17 4:31 AM
Hi,
We are using a custom board based on STM32U5G7VJTxQ and implementing USB Mass Storage Class (USBX) to expose an SD card formatted with a file system created using FileX.
The SD card when formatted with FAT32 (using FileX API), the USB mass storage device takes a very long time to become available on Windows.
Observed behavior:
Once the drive is mounted, it works normally.
We would like to understand:
Any guidance or suggestions would be appreciated.
Thank you!
2025-12-17 4:43 AM
Is this on just one Windows Host, or have you tried more?
What Windows version(s)?
@Gowri_M wrote:Any guidance or suggestions would be appreciated.
Have you tried instrumenting your code to see what's going on in your system ?
Have you tried any Windows USB diagnostic tools to see what's going on in the Host ?
Have you tried any other Hosts besides Windows?
2025-12-17 4:51 AM
Hi
We tried it on windows 10.
2025-12-17 4:59 AM
Just one single Win 10 system?
Also, what SD-Card - brand, size, etc ?
Does that card work OK in other places ?
Have you tried other SD Cards?
2025-12-17 8:43 AM
Hi,
Let me clearly explain the situation we are facing.
Initially, USB was not enabled, and we were able to perform all file operations on the SD card using the FileX API. We verified this by accessing the card through a card reader.
As the next step, we wanted our device to be recognized as a Mass Storage Class (MSC) device. For this, we enabled USBX and followed this example.
The device is detected as a mass storage device in Device Manager. However, upon connection, we immediately get a “Please insert a disk” pop-up. After approximately 3–4 minutes, the drive finally appears in File Explorer.
Answering your questions:
We tested this on two other systems, and both showed the same behavior.
The SD card used is a SanDisk Ultra microSD (32 GB).
The card works correctly in other setups; we verified this using a card reader.
We have not yet tested with other SD cards.
Thank you.
2025-12-17 8:50 AM
@Gowri_M wrote:We tested this on two other systems, and both showed the same behavior.
Were they also Win 10 systems?
Have you tried different cables, different ports, with/without hubs, etc?
Have you tried instrumenting your code to see what's going on in your system ?
Have you tried any Windows USB diagnostic tools to see what's going on in the Host ?
Have you tried any other Hosts besides Windows ?
2025-12-17 9:04 AM
Yeah both were windows 10.
Yes we tried different cables, ports and other things still the same result.
Haven't tried the last three. Will let you know once it is done.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.