2017-06-01 6:35 AM
I use STM32F429 USB HS Host library for UVC device.
Some UVC device has ISOC EP wMaxPacketSize=3072 or 5010
Bytes.
I open endpoint type iso with msp = 5010 or 3072
Then I Set Interface Alternate and start stream with
wMaxPacketSize =
5010 or 3072
I use
USBH_IsocReceiveData to receive data but USBH_LL_GetLastXferSize return max value 1020
and data image I get is missing.
I think data missing because I can't receive iso package with wMaxPacketSize =
5010.or 3072
Please me fix to receive it.
Thank you so much !!
#uvc #stm32f429 #wmaxpacketsize #usb-host-hsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.