2014-05-08 12:42 AM
Hi
I want to create custom HID device with stm32f407 and as first step I tried to rebuild the demo project for usb Mouse HID on my own, i've added needed libraries and definitions (frome demo project) and use USB_init as below to config the usb on micro, but when I connect USB to pc, after some second it says ''not usb recognized device'' anything more should I do for config the usb?#include ''stm32f4xx.h''
#include ''usbd_hid_core.h''
#include ''usbd_usr.h''
#include ''usbd_desc.h''
#include ''usbd_conf.h''
#include ''usb_conf.h''
__ALIGN_BEGIN USB_OTG_CORE_HANDLE USB_OTG_dev __ALIGN_END;
int main(void)
{
USBD_Init(&USB_OTG_dev,
USB_OTG_FS_CORE_ID,
&USR_desc,
&USBD_HID_cb,
&USR_cb);
while(1) {}
return 0;
}
thank you
#hid-usb-stm32f4-demonst
2014-05-08 1:47 AM
Hi
You have only mentioned which processor you have but you have not said which development board (assuming you are using a dev board) you have. If you have this one : http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF252419 The pre-loaded demo has HID functionality built in. Download the demo project from here : http://www.st.com/web/en/catalog/tools/PF257904# The project under 'Demonstration' should just work as a HID mouse. Alternatively, use this as a starting project and modify as needed.2014-05-08 2:35 AM
ow, I'm sorry, yes i have discovery board as you said
I found the problem just minutes ago, I forgot to use IRQ HANDLERS to send reports.now another problem I have. The structure of USB classes and drivers are so complicate, I'm going to write my own custom descriptors, and I don't understand how should I use them in this structure (usb cores, classes , ...) !?2014-05-08 2:56 AM
Hi
''The structure of USB classes and drivers are so complicate,'' Yep. ''I'm going to write my own custom descriptors,'' No, I would avoid that. It gets complicated real quick. Just modify the existing descriptors. Search the STM32 forums, there have been a few people modifying the HID mouse example with help from the forum. ''I don't understand how should I use them in this structure (usb cores, classes , ...) !?'' Try the documentation : http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882 The structure of the OTG library starts to make a little sense after reading the documentation. Certainly give big hints on which files need modifying and which to leave alone.2014-05-09 7:39 AM
thank a lot, I read that doc before, but I still don't know where should I edit descripto to create my custom HID device.
I think it's neede to read the document again.thank you2014-05-09 8:06 AM
Hi
''but I still don't know where should I edit descripto to create my custom HID device.'' The USB descriptor is 'easy'. It is in usbd_desc.c usbd_desc.h This file holds the description that is returned to the host during enumeration. What I suspect you mean is ''How do I implement the functionality of my custom HID device'' The documentation describes the layout/layers of the USB OTG driver. Hints at which files need to be modified (for USH Host or USB Device - HID is a USB Device). Also Search this forum, I know a cuple of others have asked about implementing joypad HID2014-05-09 9:38 AM
Just last question, I promise :D
I found descriptor and its clear, now after modifying that, I want to send my reports to PC by ''USBD_HID_SendReport()'' function. is it create report automatically (in class functions & etc) and its I should just return buffer of data to it? or I should myself create the report?
thank you much more ;)2014-05-09 10:04 AM
Hi
''Just last question, I promise :D'' No problems. Feel free to ask (sensible) questions. ''I want to send my reports to PC by ''USBD_HID_SendReport()'' function. is it create report automatically (in class functions & etc) and its I should just return buffer of data to it? or I should myself create the report?
'' It looks like the function is provided by the core library for USB HID I am afraid that I have not tried a HID device myself so I cannot say from experience. The document (UM1021 STM32F105xx, STM32F107xx, STM32F2xx and STM32F4xx USB On-The-Go host and device library) states : ''The USBD_HID_SendReport can be used by the application to send HID reports, the HID driver, in this release, handles only IN traffic.'' so my guess is that you just call the function and pass your data in. Again, search this forum. I know some others have been asking about USB HID2014-05-09 11:36 AM
I think I found answer of all my questions now.
here I found good description about HID packets: http://www.usbmadesimple.co.uk/ums_5.htmand in this page, I found my last questions answer :http://www.usbmadesimple.co.uk/ums_ms_desc_conf.htmafter introduce HID device to host, it's just needed to send data as described in ''Device Descriptor
'' before.thank a lot for your patience and help. Now I think I'm ready to start my custom HIDWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.