2013-08-28 2:05 PM
I own a stm32f4 discovery board, for which a demonstration project can be downloaded here:
http://www.st.com/web/en/catalog/tools/PF257904
This demo consists of software to use the board as a usb hid mouse, using the accelerometer to control the mouse movement. I now want to change this into a gamepad, for now I'm leaving the other parts of the descriptor the same, so I only changed the usage from 0x09,0x02 (usage: mouse)
to 0x09 , 0x09 (usage: gamepad). (these values can be found in the usb_hid_core file)
But after this change the computer still sees it as a mouse, but one that is not functioning correctly. What else should I change?
Any help would be greatly appreciated, I have been trying all kinds of things, but nothing seems to work.
I have included the file that I linked to, the usb_hid_core file can be found in this file at this location: stsw-stm32068\STM32F4-Discovery_FW_V1.1.0\Libraries\STM32_USB_Device_Library\Class\hid\src #stm32f4-hid-mouse-gamepad2013-09-02 7:16 AM
Nobody?
2013-09-02 6:36 PM
Evidently
It's also not appropriate to attach a copy of a 31 MB file to the forum, where a would be quite adequate. Your files, or a patch, would be far more effective.2013-09-03 8:19 AM
Thanks for the tip.
I'm still stuck, i managed to alter the mouse descriptor, but can't get it to work as a gamepad, this is what my analyzer tells me:2013-09-04 2:16 PM
Try this descriptor instead
0x05, 0x01, // USAGE_PAGE (Generic Desktop) 0x09, 0x05, // USAGE (Gamepad) // use 0x09, 0x04 for USAGE (Joystick) 0xa1, 0x01, // COLLECTION (Application) 0xa1, 0x00, // COLLECTION (Physical) 0x09, 0x30, // USAGE (X) 0x09, 0x31, // USAGE (Y) 0x15, 0x81, // LOGICAL_MINIMUM (-127) 0x25, 0x7f, // LOGICAL_MAXIMUM (127) 0x75, 0x08, // REPORT_SIZE (8) 0x95, 0x02, // REPORT_COUNT (2) 0x81, 0x02, // INPUT (Data,Var,Abs) 0xc0, // END_COLLECTION 0xa1, 0x00, // COLLECTION (Physical) 0x09, 0x32, // USAGE (Z) // use 0x09, 0x30 for USAGE (X) // use 0x09, 0x33 for USAGE (Rx) 0x09, 0x35, // USAGE (Rz) // use 0x09, 0x31 for USAGE (Y) // use 0x09, 0x34 for USAGE (Ry) 0x15, 0x81, // LOGICAL_MINIMUM (-127) 0x25, 0x7f, // LOGICAL_MAXIMUM (127) 0x75, 0x08, // REPORT_SIZE (8) 0x95, 0x02, // REPORT_COUNT (2) 0x81, 0x02, // INPUT (Data,Var,Abs) 0xc0, // END_COLLECTION 0xa1, 0x00, // COLLECTION (Physical) 0x05, 0x09, // USAGE_PAGE (Button) 0x19, 0x01, // USAGE_MINIMUM (Button 1) 0x29, 0x10, // USAGE_MAXIMUM (Button 16) 0x15, 0x00, // LOGICAL_MINIMUM (0) 0x25, 0x01, // LOGICAL_MAXIMUM (1) 0x75, 0x01, // REPORT_SIZE (1) 0x95, 0x10, // REPORT_COUNT (16) 0x81, 0x02, // INPUT (Data,Var,Abs) 0xc0, // END_COLLECTION 0xc0 // END_COLLECTION2013-09-07 9:19 AM
I tried it, but is still shows as a non functional mouse. I went trough all the files, but I can't find anything, is there a common reason why just changing the usage page and nothing else might not work?
2013-09-22 5:06 AM
Nobody?
2014-04-12 1:56 PM
2014-05-05 10:56 AM
You need to change few others things to make it work as a gamepad. In usbd_hid_core.c you need to change :
0x02, //nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse to the 0x00 value. Other thing, the report descriptor has to be changed, this is mine for a 3-buttons 2-axis gamepad, (you can change it to add button or anything else with the HIDtool) : __ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_END = { 0x05, 0x01, // USAGE_PAGE (Generic Desktop) 0x09, 0x05, // USAGE (Game Pad) 0xA1, 0x01, // COLLECTION (Application) 0xA1, 0x00, // COLLECTION (Physical) 0x05, 0x09, // USAGE_PAGE (Button) 0x19, 0x01, // USAGE_MINIMUM (Button 1) 0x29, 0x03, // USAGE_MAXIMUM (Button 3) 0x15, 0x00, // LOGICAL_MINIMUM (0) 0x25, 0x01, // LOGICAL_MAXIMUM (1) 0x95, 0x03, // REPORT_COUNT (3) 0x75, 0x01, // REPORT_SIZE (1) 0x81, 0x02, // INPUT (Data,Var,Abs) 0x95, 0x01, // REPORT_COUNT (1) 0x75, 0x05, // REPORT_SIZE (5) 0x81, 0x07, // INPUT (Cnst,Var,Rel) 0x05, 0x01, // USAGE_PAGE (Generic Desktop) 0x09, 0x30, // USAGE (X) 0x09, 0x31, // USAGE (Y) 0x15, 0x81, // LOGICAL_MINIMUM (-127) 0x25, 0x7F, // LOGICAL_MAXIMUM (127) 0x75, 0x08, // REPORT_SIZE (8) 0x95, 0x02, // REPORT_COUNT (2) 0x81, 0x02, // INPUT (Data,Var,Abs) 0xC0, 0xC0 // END_COLLECTION x2 }; The size of the report descriptor has changed so modify it in usbd_hid_core.c : #define HID_MOUSE_REPORT_DESC_SIZE 48 Now the gamepad would be recognized. You only need to send a 3 bytes report (the first for the button, et the two others for the axis). For a test you could do it by using this code in stm32xx_it.c : static uint8_t *USBD_HID_GetPos (void) { static uint8_t HID_Buffer[3] = {0}; static int8_t val_abs_x=0; static uint8_t sens_x=0; HID_Buffer[1] = 0; HID_Buffer[2] = 0; // X move if (val_abs_x > 120) { sens_x = 0; // -- HID_Buffer[0]=0; } else if (val_abs_x < -120) { sens_x = 1; // ++ HID_Buffer[0]=1; } if (sens_x == 1) val_abs_x = val_abs_x + 3; else val_abs_x = val_abs_x - 3; HID_Buffer[1] = val_abs_x; HID_Buffer[2] = 0; return HID_Buffer; } Anf finally change the line (in the same file) : USBD_HID_SendReport (&USB_OTG_dev, buf, 4); to : USBD_HID_SendReport (&USB_OTG_dev, buf, 3); This should work well on the STM32f4 discovery board. If not try change the PID by adding 1 (like 0x5711) in usbd_desc.c.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.