2020-08-14 6:53 AM
Hello everybody,
I need some helps regarding a trouble with my USB project.
I have developed a project base on MXCube with a composite MSC and CDC. When I launch the software it works perfectly (which means that I have the mass storage and the port com avaialble).
Now two use cases:
Something should be missing if a portcom is not opened but I don't know what….
2020-08-15 3:33 AM
Hi,I am trying to do the same composite project that you did,but I can not make the MSC project work with IDMA and cache,it can only work when cache and IDMA not use.Do your MSC project use the IDMA and cache?
My project's Issue detail:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.