2016-07-11 5:55 AM
Hello!
I use the USB CDC class implementation provided by STM32CubeMX 4.10.1 (firmware library v1.3.0) with stm32l0x3 and I try to get a composite device with multiply VCP ports. I'm rather not interested in changes in descriptors, because they are described everywhere. Much more interesting are changes in all objects and structures which are in this inmplementation and all places which are necessary to handle transmission with 2 or 3 VCP. Can anyone help me with this?Regards,Micha? #stm32-usb-cdc-vcp2016-12-28 5:45 AM
Hi
Michał,
For STM32F072xx controller even if I
changes in descriptors but still it is not detecting as 2 virtual com port.
Please can you help were exactlyI need to modify.
Currently inDescriptor I modified
0xEF, /*bDeviceClass*/
0x02, /*bDeviceSubClass*/
0x01, /*bDeviceProtocol*/
#if defined ( __ICCARM__ ) /*!< IAR Compiler */
#pragma data_alignment=4
#endif
/* USB Standard Device Descriptor */
__ALIGN_BEGIN uint8_t USBD_FS_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END =
{
0x12, /*bLength */
USB_DESC_TYPE_DEVICE, /*bDescriptorType*/
#if (USBD_LPM_ENABLED == 1)
0x01, /*bcdUSB */ /* changed to USB version 2.01
in order to support LPM L1 suspend
resume test of USBCV3.0*/
#else
0x00, /* bcdUSB */
#endif
0x02,
0xEF, /*bDeviceClass*/
0x02, /*bDeviceSubClass*/
0x01, /*bDeviceProtocol*/
USB_MAX_EP0_SIZE, /*bMaxPacketSize*/
LOBYTE(USBD_VID), /*idVendor*/
HIBYTE(USBD_VID), /*idVendor*/
LOBYTE(USBD_PID_FS), /*idVendor*/
HIBYTE(USBD_PID_FS), /*idVendor*/
0x00, /*bcdDevice rel. 2.00*/
0x02,
USBD_IDX_MFC_STR, /*Index of manufacturer string*/
USBD_IDX_PRODUCT_STR, /*Index of product string*/
USBD_IDX_SERIAL_STR, /*Index of serial number string*/
USBD_MAX_NUM_CONFIGURATION /*bNumConfigurations*/
} ;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2016-12-30 7:20 AM
Dear
,You may refer to this manual which can help you on USB VCP device
You should use the latest version of CubeMx v4.18.0 and firmware package (STM32CubeL0 v1.8.0) which contains fix defects and enhancements implementation.
Happy New Year
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.