2014-04-11 1:07 AM
Hey everybody,
in order to initialize a working Virtual Com Port with CubeMX on the STM32F4 Discovery, I had to changepdev->pClassData = USBD_malloc(sizeof (USBD_CDC_HandleTypeDef));
topdev->pClassData = (void *) USBD_malloc(sizeof (USBD_CDC_HandleTypeDef));
Without the type cast pClassData would always be null, which will make the parent function (USBD_CDC_Init in usbd_cdc.c) return before initializing the interface. Btw I used firmware 1.1.0.EDIT: Sorry, that was too fast. This line was actually not the root cause, it was the following line in USB_CDC.h &sharpdefine CDC_DATA_HS_MAX_PACKET_SIZE 512Changing that value to 256 made it work for me now. In case anyone is interested, here's a small code example for a vcp mirror. Add this code to CDC_Receive in usb_cdc_if.c
static uint8_t buff_RX[256];
static uint8_t buff_TX[256]; int i = 0; for (i = 0; i < *Len; i++) buff_TX[i] = buff_RX[i]; USBD_CDC_SetTxBuffer(&hUsbDeviceFS, &buff_TX[0], *Len); USBD_CDC_TransmitPacket(&hUsbDeviceFS); USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &buff_RX[0]); USBD_CDC_ReceivePacket(&hUsbDeviceFS);Also you will have to add
extern USBD_HandleTypeDef hUsbDeviceFS;
to this file.
#usb #cdc #cdc #cdc #cdc_receive_fs #full-echo #usb-cdc #vcp #vcp2014-05-13 1:50 AM
Hi Ramdas,
I have generated the basis for the project by CubeMXIn my case the function CDC_Init(void) is also empty.It works in spite of this.But you can add your code if you need.2014-05-13 9:24 PM
hi Andrii,
thanks for the reply. currently the PC is detecting the device but if i see in the device manager there is yellow exclamatory saying the following message ''This device cannot start. (Code 10)'' seems like the code which i flashed is not handling the SOF correctly.please could you share me your STM32CubeMX and the keil project. i am using a Win7 PC.Thanks in advance.Ramdas2014-05-14 4:29 AM
2014-05-14 5:05 PM
/* Private function prototypes -----------------------------------------------*/
static
void
SystemClock_Config(
void
);
uint8_t cdc_activity;
int
main(
void
)
{
/* USER CODE BEGIN 1 */
cdc_activity = 0;
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
// MX_ADC3_Init();
MX_CRC_Init();
// MX_DAC_Init();
MX_FMC_Init();
MX_RNG_Init();
// MX_SDIO_SD_Init();
// MX_SPI4_Init();
// MX_TIM6_Init();
// MX_USART1_UART_Init();
MX_USB_DEVICE_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/*## FatFS: Link the SD disk I/O driver ###############################*/
// SD_DriverNum = FATFS_LinkDriver(&SD_Driver, SD_Path);
/* USER CODE BEGIN 3 */
/* Infinite loop */
while
(1)
{
Led_Red_Toggle();
HAL_Delay(125);
if
( cdc_activity )
{
cdc_activity--;
Led_Green_Toggle();
}
}
/* USER CODE END 3 */
} Notice I disabled any unused (for the time being) peripherals. I'm not planning to use the LCD for my tests but this is another story. and the ''modified'' CDC_Receive()
extern
uint8_t cdc_activity;
static
int8_t CDC_Receive (uint8_t* Buf, uint32_t *Len)<br>
{
/* USER CODE BEGIN 7 */
cdc_activity = (uint8_t)*Len;
return
(USBD_OK);
/* USER CODE END 7 */
}
I haven't found the problem yet. It's late, I'm tired, and calling it a night. Best luck tomorrow, maybe. Also, I noticed something strange in the CDC_Init() method : static
int8_t CDC_Init(
void
)
{
hUsbDevice_0 = &hUsbDeviceHS;
/* USER CODE BEGIN 4 */
/* Set Application Buffers */
USBD_CDC_SetTxBuffer(hUsbDevice_0, UserTxBuffer, 0);
// <-- shouldn't this receive APP_TX_DATA_SIZE as its last argument ?
USBD_CDC_SetRxBuffer(hUsbDevice_0, UserRxBuffer);
return
(USBD_OK);
/* USER CODE END 4 */
} Shouldn't the USBD_CDC_SetTxBuffer() method be called with APP_TX_DATA_SIZE as its last argument ?
________________
Attachments : Repetier429I.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzOT&d=%2Fa%2F0X0000000bL7%2Fs0P1zgKv_wXg3uvZchnDQjLJYY1jUVEFnMU1hmtWoUI&asPdf=false
2014-05-14 7:48 PM
hi Andril,
i now solved the issue with richard's solution. so to bother you all. now it communicates once, let me test it fully and then come share my experience.thanks to all ,Ramdas2014-05-15 5:12 AM
2014-05-16 1:36 AM
Hi jla
Check your clocks very carefully. In another post (Windows 7 CDC) I solved a clock related issue.The divisors I used were 8MHz HSE, Divide 8, PLL 336, divide 7 this works Divide 8, PLL 192, divide 4 does not work even though it generates 48MHzAlso check VBUS and SOF are correct for your hardwareIf you have an ST board, tru use cube to generate a project and run it, then compare to what is not workingChris2014-05-16 4:46 AM
/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/USB%20middleware%20issue%20with%20CDCVCP%20only%20x%20packets%20receivable%20%28HAL%1.0%20and%20Host-Device_Lib%1.0%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=162
to set/reset the pdev->pClassData->TxState flag after each IN (host-wise) packet now : 1) Added his implementation of USB_EpTxCount(..) o stm32f4xx_ll_usb.c 2) Added his implementation of HAL_PCD_EP_GetTxCount(..) to stm32f4xx_hal_pcd.c 3) Added his implementation of USBD_LL_GetTxCount(..) to usbd_conf.h 4) Modified USBD_CDC_TransmitPacked(..) from usbd_cdc.c like so :
uint8_t USBD_CDC_TransmitPacket(USBD_HandleTypeDef *pdev)
{
USBD_CDC_HandleTypeDef *hcdc = pdev->pClassData;
if
(pdev->pClassData != NULL)
{
if
(hcdc->TxState == 0)
{
/* Transmit next packet */
USBD_LL_Transmit(pdev,
CDC_IN_EP,
hcdc->TxBuffer,
hcdc->TxLength);
/* Tx Transfer in progress */
hcdc->TxState = 1;
return
USBD_OK;
}
else
{
return
USBD_BUSY;
}
}
else
{
return
USBD_FAIL;
}
}
becomes :
extern
uint32_t USBD_LL_GetTxCount (USBD_HandleTypeDef *pdev, uint8_t ep_addr);
uint8_t USBD_CDC_TransmitPacket(USBD_HandleTypeDef *pdev)
{
USBD_CDC_HandleTypeDef *hcdc = pdev->pClassData;
if
(pdev->pClassData != NULL)
{
if
(hcdc->TxState == 0)
{
/* Transmit next packet */
USBD_LL_Transmit(pdev,
CDC_IN_EP,
hcdc->TxBuffer,
hcdc->TxLength);
/* Tx Transfer in progress */
hcdc->TxState = USBD_LL_GetTxCount(pdev,CDC_IN_EP) ? 1 : 0;
return
USBD_OK;
}
else
{
return
USBD_BUSY;
}
}
else
{
return
USBD_FAIL;
}
}
Works (almost) like a charm now :
The loopback is still getting some bytes stuck in the device-side transmit buffer, so I'll look into it as soon as I have time for it. I did not look at his code hard enough to detect any flaw, but again, I'm pretty busy with other things right now.
Still, one step further is a good one.
2014-05-28 9:03 PM
hi Jla,
here is my code which works fine.static int8_t CDC_Init(void){ /* USER CODE BEGIN 3 */ USBD_CDC_SetTxBuffer(&hUsbDeviceFS, &buff_TX[0],256); USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &buff_RX[0]); return (0); /* USER CODE END 3 */ }static int8_t CDC_Receive (uint8_t* Buf, uint32_t *Len){ /* USER CODE BEGIN 6 */ if(pack_processed==0) { pak_len = *Len; USBD_CDC_ReceivePacket(&hUsbDeviceFS); pack_received=1; } return (0); /* USER CODE END 6 */ } and then in the mail just for testing , i was using the following code. /* USER CODE BEGIN 3 */ /* Infinite loop */ while (1) { if(pack_received == 1) { if(pak_len == 4) { if((buff_RX[0]=='1')&&(buff_RX[1]=='2')&&(buff_RX[2]=='3')&&(buff_RX[3]=='4')) { strcpy((char *)buff_TX,''Received1234\n\r>''); USBD_CDC_SetTxBuffer(&hUsbDeviceFS, &buff_TX[0], strlen(''Received1234\n\r>'')-1); // it is important to send the ''/n/r>'' otherwise the driver will hang. USBD_CDC_TransmitPacket(&hUsbDeviceFS); } } pack_processed=0; pack_received=0; } } /* USER CODE END 3 */i hope it helps you, and one more thing please do not forget to do the change that Richard was saying the earlier post in the file make sure the macro is 256 otherwise the class is not getting created. may because of heap size or stack size. i think there is a information on the same in this post.#define CDC_DATA_HS_MAX_PACKET_SIZE 256 /* Endpoint IN & OUT Packet size */good luck,Ramdas2014-06-13 5:39 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.