2021-07-04 1:05 AM
Hi,
I have already ported the USB AUDIO DAC application code to STM32F401VC Discovery board. After running the application I am getting noisy audio output from the codec.
Please check it & inform me if you found any mistake(it could be in configuration or audio sync or any other problem) .
And I have also attached the project file.
IDE KEIL MDK ARM
STM32F401VC Discovery Board
Thanks & Regards
Satyabrata Senapati
2021-07-12 2:13 AM
Hello @ssena.1514 ,
I recommend that you try to start with the example provided under our F4 firmware package and update it as needed.
The example is provided under this path: Firmware\Projects\STM32F401-Discovery\Applications\Audio\Audio_playback_and_record
I hope this helps you.
BeST Regards,
Walid
2021-07-12 2:40 AM
Thanks for replying....
Actually there is no such example for stm32f401vc discovery board.But for stm32f407 there is such an example. I have also ported this playback & record application to 401 board and it's working fine.
But when I am porting the usb audio example from usb library it's not working correctly(noisy).
I have already verified the application & don't know where is the fault actually.
Whether the fault is in codec or usb side.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.