2023-03-14 8:42 AM
Hallo, I'm using the Nucleo board for STM32U5, LL drivers for USART1 and DMA.
in my main.c the init function are:
static const char
long_string[] = ""
"What's the problem"
"???????\r\n"
"";
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_DMA_InitTypeDef DMA_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
/**USART1 GPIO Configuration
PA9 ------> USART1_TX
PA10 ------> USART1_RX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_9|LL_GPIO_PIN_10;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_DOWN;
GPIO_InitStruct.Alternate = LL_GPIO_AF_7;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USART1 DMA Init */
/* GPDMA1_REQUEST_USART1_TX Init */
DMA_InitStruct.SrcAddress = (uint32_t)long_string;
DMA_InitStruct.DestAddress = 0x00000000U;
DMA_InitStruct.Direction = LL_DMA_DIRECTION_MEMORY_TO_PERIPH;
DMA_InitStruct.BlkHWRequest = LL_DMA_HWREQUEST_SINGLEBURST;
DMA_InitStruct.DataAlignment = LL_DMA_DATA_ALIGN_ZEROPADD;
DMA_InitStruct.SrcBurstLength = 1;
DMA_InitStruct.DestBurstLength = 1;
DMA_InitStruct.SrcDataWidth = LL_DMA_SRC_DATAWIDTH_BYTE;
DMA_InitStruct.DestDataWidth = LL_DMA_DEST_DATAWIDTH_BYTE;
DMA_InitStruct.SrcIncMode = LL_DMA_SRC_INCREMENT;
DMA_InitStruct.DestIncMode = LL_DMA_DEST_FIXED;
DMA_InitStruct.Priority = LL_DMA_LOW_PRIORITY_LOW_WEIGHT;
DMA_InitStruct.BlkDataLength = 10;
DMA_InitStruct.TriggerMode = LL_DMA_TRIGM_BLK_TRANSFER;
DMA_InitStruct.TriggerPolarity = LL_DMA_TRIG_POLARITY_MASKED;
DMA_InitStruct.TriggerSelection = 0x00000000U;
DMA_InitStruct.Request = LL_GPDMA1_REQUEST_USART1_TX;
DMA_InitStruct.TransferEventMode = LL_DMA_TCEM_BLK_TRANSFER;
DMA_InitStruct.SrcAllocatedPort = LL_DMA_SRC_ALLOCATED_PORT0;
DMA_InitStruct.DestAllocatedPort = LL_DMA_DEST_ALLOCATED_PORT0;
DMA_InitStruct.LinkAllocatedPort = LL_DMA_LINK_ALLOCATED_PORT1;
DMA_InitStruct.LinkStepMode = LL_DMA_LSM_FULL_EXECUTION;
DMA_InitStruct.LinkedListBaseAddr = 0x00000000U;
DMA_InitStruct.LinkedListAddrOffset = 0x00000000U;
LL_DMA_Init(GPDMA1, LL_DMA_CHANNEL_0, &DMA_InitStruct);
/* USART1 interrupt Init */
NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 1));
NVIC_EnableIRQ(USART1_IRQn);
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
USART_InitStruct.PrescalerValue = LL_USART_PRESCALER_DIV1;
USART_InitStruct.BaudRate = 115200;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_SetTXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_SetRXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_DisableFIFO(USART1);
LL_USART_ConfigAsyncMode(USART1);
LL_USART_Enable(USART1);
/* USER CODE BEGIN USART1_Init 2 */
LL_USART_EnableIT_TC(USART1);
LL_DMA_EnableIT_HT(GPDMA1, LL_DMA_CHANNEL_0);
LL_DMA_EnableIT_TC(GPDMA1,LL_DMA_CHANNEL_0);
LL_DMA_EnableIT_USE(GPDMA1, LL_DMA_CHANNEL_0);
LL_DMA_EnableIT_ULE(GPDMA1, LL_DMA_CHANNEL_0);
LL_DMA_EnableIT_DTE(GPDMA1, LL_DMA_CHANNEL_0);
LL_USART_EnableDMAReq_TX(USART1);
LL_DMA_EnableChannel(GPDMA1, LL_DMA_CHANNEL_0);
/* USER CODE END USART1_Init 2 */
}
LL_DMA_IsActiveFlag_DTE becomes active.
What am I doing wrong?
Thnak you
Any help would be appreciated.
It was missing this
DMA_InitStruct.DestAddress = LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_TRANSMIT);
Solved! Go to Solution.
2023-03-17 6:19 AM
Hi @IVent.1
DTEF Flag is set when executing the data transfer from register file fail. You have to check if your DMA Channel is correctly enabled and if you have properly configured your DMA( Destination,...).
Regards
DianeP
2023-03-17 6:19 AM
Hi @IVent.1
DTEF Flag is set when executing the data transfer from register file fail. You have to check if your DMA Channel is correctly enabled and if you have properly configured your DMA( Destination,...).
Regards
DianeP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.