2019-07-15 11:01 AM
I read some related topics on this community but none of them could fixes the issue.
I'm currently trying to disable a USB OUT endpoint (following the steps from the Reference Manual) but the Global NAK Effective interrupt bit (GONAKEFF in USB_OTG_FS_GINTSTS) is never set, after I set the USB_OTG_DCTL_SGONAK bit in USB_OTG_FS_DEVICE_DCTL while the interrupt is masked (as it is supposed to be, according to the doc). Is there some thing I'm missing to disable properly the endpoint ?
Thank you in advance
2023-01-19 4:50 AM
I had same problem with STM32F7 (HAL version 1.16.0).
Found interesting comment in NuttX source code (stm32_otgdev.c)
/* Wait for the GONAKEFF interrupt that indicates that the OUT NAK
* mode is in effect. When the interrupt handler pops the OUTNAK word
* from the RxFIFO, the core sets the GONAKEFF interrupt.
*/
/* Since we are in the interrupt handler, we cannot wait inline for the
* GONAKEFF because it cannot occur until service the RXFLVL global interrupt
* and pop the OUTNAK word from the RxFIFO.I tried to manually flush RxFifo (while in ISR) with this code and eventually got BOUTNAKEFF set (GONAKEFF is defined as BOUTNAKEFF in HAL libraries)
if ((USB_OTG_HS->GINTSTS & USB_OTG_GINTSTS_BOUTNAKEFF) == 0)
{
((USB_OTG_DeviceTypeDef *)(USB_OTG_HS_PERIPH_BASE + USB_OTG_DEVICE_BASE))->DCTL = USB_OTG_DCTL_SGONAK;
while ((USB_OTG_HS->GINTSTS & USB_OTG_GINTSTS_BOUTNAKEFF) == 0)
{
if (USB_OTG_HS->GINTSTS & USB_OTG_GINTSTS_RXFLVL)
{
uint32_t temp = USBx->GRXSTSP;
while (USB_OTG_HS->GINTSTS & USB_OTG_GINTSTS_RXFLVL)
temp = USBx->GRXSTSP;
}
}
/* ... */
((USB_OTG_DeviceTypeDef *)(USB_OTG_HS_PERIPH_BASE + USB_OTG_DEVICE_BASE))->DCTL = USB_OTG_DCTL_CGONAK;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.