2021-05-22 5:39 AM
Hi,
Am trying to create the ASC model which is existing in FP-AI-SENSING1 Pack. When I was converting from keras model to TFlite model am getting below error. Am using the same code which is in the pack, am not changing anything. Even the audio files am using the same.
Anyone can help?
ERROR-
AttributeError: type object 'TFLiteConverter' has no attribute 'from_keras_model'
Below is the code which am using to convert into TFlite model.
def representative_dataset_gen():
for i in range(len(x_train_r)):
yield [x_train_r[i].reshape((1, ) + x_train_r[i].shape)]
converter = tf.lite.TFLiteConverter.from_keras_model(out_dir + "Outputmodel.h5" )
converter.optimizations = [tf.lite.Optimize.DEFAULT]
converter.representative_dataset = representative_dataset_gen
converter.target_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]
converter.inference_input_type = tf.int8
converter.inference_output_type = tf.int8
tflite_model = converter.convert()
with open(out_dir + 'model.tflite','wb') as f:
f.write(tflite_model)
print("TFlite model saved")
Regards,
shankari.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.