2013-11-13 1:54 AM
Hi everybody,
I was very happy to see uCLinux port for Cortex-M4 and my favorite MCU STM32. This well done job was achieved by emcraft. So I wonder that is it possible to run uCLinux on my new toy STM32F429I-DISCO? I have started for it and some u-boot and kernel patching I finished my first job. You must known that code execution from SDRAM on STM32F4 much slower than from FLASH (~6x times slower). So in fact this core is not suitable code execution from SDRAM. But maybe you don't have any chance so you can accept this penalty. Than I modified the kernel to load romfs from flash, simple frame buffer driver, u-boot patching for SDRAM and LCD init functions. You can try and decide for yourself. This is boot-up and simple framebuffer demo video. Emcraft original source git is https://github.com/EmcraftSystems (not including STM32F429I-DISCO board drivers)Sample image attached to the post. This image contains u-boot, kernel and romfs. The serial console is USART3 and PC10->MCU TX, PC11->MCU RX. Don't forget that this interface has TTL levels. #usart #stm32-uclinux-u-boot #usb-driver-p19-stm324f2014-01-19 11:02 AM
Hi
@tmk, in /usr/bin is located program extract, is required when system boots. Can You share source code of this file? I try to compile kernel and busybox with libraries from uClibc and probably this program crashes system boot. Last 2 messages from system is : VFS: Mounted root (...) readonly on device Freeing init memory: 16K and end Do I need also compile ram disc and how to do it? Has somebody recipe for enable pthreads? Thank you for all2014-01-28 6:57 AM
Thank you BIG time for your enormous effort.
I used your complete hex image and it works as expected, but I do have a problem with the serial communication.I have connected my stm32f429i-disco board to a breadboard with a HIN202ECBZ to convert the USART3 lines (PC10=MCU_TX, PC11=MCU_RX) to RS232 levels. When connecting a serial terminal monitor (tried on linux and on windows with 115200,8n1) I receive all the boot up messages, but I am unable to send anything. Therefore I am not able to login or anything. Sometimes aftre pressing random keys some garbage (as if the baudrate would not match) appears in the terminal. Could it be, that PC11 is already used for something else?I would claim that my HIN202 circuit is correct. Does anybody have a hint as to what the problem could be?2014-02-09 5:46 AM
hi all,
If you prefer to use Linux as host, you can consider the simple tool designed to create a uClinux distribution for STM32f429 Discovery board: Just have to 'make' and 'make install'. Then, the builder will fetch and compile u-boot, linux kernel, and busybox from scratch.2014-02-13 6:34 PM
2014-02-14 3:17 PM
Hi tmk,
What are the terms of use for the LCD display driver code you have copyrighted ? Under what terms can we use it in projects ? Thanks!2014-03-02 10:59 AM
when I tried to build the image I got an error saying ''
u-boot.lds:9: nonconstant expression for origin'' and line 9 has : ''
RAM_BUF (r): ORIGIN = (ORIGIN(RAM) + LENGTH(RAM)), LENGTH = (88 * 1024)
''anyone has an idea what might the problem be?
2014-03-10 3:47 AM
Hi
I have a question regarding the USB OTG function. Is a USB to Ethernet dongle supported? This would be a really cool feature if I can connect the STM32F429 to ethernet. I think this is easier than connecting a phy to the STM32 that needs some modification to the DISCO board. Best regards2014-06-01 6:50 AM
Dear All,
Tayfun Mehmet Karan (aka tmk), Jim Huang (aka jserv) and all developers of Emcraft Systems: Just to let you know that your present porting of ucLinux on the STM32F429i-Discovery has been reciently introduced and published in a french Embedded Software magazine called ''Open Silicium'' #11 of June-July-August 2014 http://www.unixgarden.com/index.php/open-silicium/open-silicium-n11-juin-juillet-aout-2014-en-kiosque Best regards, Thierry2014-06-12 3:57 PM
Does anyone know of the Linux support for the USB device with P19 USB OTG on the STM324F SOM eval board?
2014-06-12 4:01 PM
Hi. Does anyone know of a Linux driver for the USB device with P19 USB OTG on the STM324F SOM eval board from emCraft?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.