2013-11-13 1:54 AM
Hi everybody,
I was very happy to see uCLinux port for Cortex-M4 and my favorite MCU STM32. This well done job was achieved by emcraft. So I wonder that is it possible to run uCLinux on my new toy STM32F429I-DISCO? I have started for it and some u-boot and kernel patching I finished my first job. You must known that code execution from SDRAM on STM32F4 much slower than from FLASH (~6x times slower). So in fact this core is not suitable code execution from SDRAM. But maybe you don't have any chance so you can accept this penalty. Than I modified the kernel to load romfs from flash, simple frame buffer driver, u-boot patching for SDRAM and LCD init functions. You can try and decide for yourself. This is boot-up and simple framebuffer demo video. Emcraft original source git is https://github.com/EmcraftSystems (not including STM32F429I-DISCO board drivers)Sample image attached to the post. This image contains u-boot, kernel and romfs. The serial console is USART3 and PC10->MCU TX, PC11->MCU RX. Don't forget that this interface has TTL levels. #usart #stm32-uclinux-u-boot #usb-driver-p19-stm324f2014-01-07 4:52 AM
2014-01-09 1:34 AM
Hi. I'm totally newbe for uClinux and for STM platform. Is possible to write more information about uClinux here.. what all command is possible to use , and if support any USB mass storage or SD card ?? and how to write easy small program (for example hellow world ) in Windows PC ?? best regards..
2014-01-09 6:41 AM
This seems a bit remedial for this thread, suggest you start a new one if you are looking for tutorials and basic stuff. I'd also suspect you could find a lot of this type of stuff with a Google/Bing search.
2014-01-09 6:56 AM
Ehm.. yes. but if try searching in google .. stm32f429 + linux show only this web forum.. hehe.. I ned only small help ..
ok .. thanks for all .. best regards.2014-01-11 1:28 AM
Hi.Today I try install and compile files for uClinux.
I use scripts from gore.mike but had problem to do it.. after install or compile say error.. What I do : 1. To my WIn7 64-bit install Oracle VM and to this VM install Ubuntu 12.04 LTS 64-bit version 2. in home directory create new directory with name uCLinux 3. download all scripts from gore.mike and unzip to my uCLinux directory 4. open terminal and start run step by step run scripts 5. ./setvarsPATH:[/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games]
6. /install_uclinuxupdating: install_libusbx (deflated 40%)
updating: install_packages (deflated 29%) updating: install_stlink (deflated 57%) updating: install_tools (deflated 35%) updating: install_uclinux (deflated 51%) updating: flash_uclinux (deflated 60%) updating: setvars (deflated 32%) updating: readme.txt (deflated 55%) PATH:[/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games] updating package list - this may take a while E: Could not open lock file /var/lib/dpkg/lock - open (13: Permission denied) E: Unable to lock the administration directory (/var/lib/dpkg/), are you root? PATH:[/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games] File `arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2' already there; not retrieving. tar (child): arm-arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2: Cannot open: No such file or directory tar (child): Error is not recoverable: exiting now tar: Child returned status 2 tar: Error is not recoverable: exiting now PATH:[/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games] updating package list - this may take a while E: Could not open lock file /var/lib/dpkg/lock - open (13: Permission denied) E: Unable to lock the administration directory (/var/lib/dpkg/), are you root? /usr/bin/install: /usr/bin/install: cannot execute binary file install_stlink: line 31: git: command not found install_stlink: line 36: pushd: stlink: No such file or directory install_stlink: line 41: ./autogen.sh: No such file or directory install_stlink: line 42: ./configure: No such file or directory make: *** No targets specified and no makefile found. Stop. make: *** No rule to make target `install'. Stop. ==== install_stlink: line 56: [: /etc/udev/rules.d/70-persistent-cd.rules: binary operator expected root privileges required ==== install_stlink: line 64: pushd: src: No such file or directory Compile tests gcc: error: test_usb.c: No such file or directory gcc: error: ../libstlink.a: No such file or directory gcc: error: /usr/local/lib/libusb-1.0.a: No such file or directory gcc: error: test_usb.c: No such file or directory gcc: error: ../libstlink.a: No such file or directory gcc: error: /usr/local/lib/libusb-1.0.a: No such file or directory install_stlink: line 72: popd: directory stack empty install_stlink: line 74: popd: directory stack empty get u-boot https://github.com/robutest/u-boot ./install_uclinux: line 38: git: command not found get uclinux https://github.com/robutest/uclinux ./install_uclinux: line 38: git: command not found get stm32-bins https://github.com/robutest/stm32-bins ./install_uclinux: line 38: git: command not found ./install_uclinux: line 43: pushd: u-boot: No such file or directory building stlink with libusbx package make: *** No rule to make target `stm32429-disco'. Stop. make: *** No rule to make target `tools'. Stop. ./install_uclinux: line 47: popd: directory stack empty ./install_uclinux: line 50: pushd: uclinux: No such file or directory Modify default robutest uclinux configuration ? y/n [n]: 7.set: y and ENTER 8. result:make: *** No rule to make target `mrproper'. Stop.
cp: cannot stat `config.robutest': No such file or directory Running menuconfig - just save configuration - no need to chang enything make: *** No rule to make target `menuconfig'. Stop. building uclinux make: *** No targets specified and no makefile found. Stop. ./install_uclinux: line 70: pushd: arch/arm/boot: No such file or directory ./install_uclinux: line 71: make_uboot_ximage: command not found ./install_uclinux: line 72: popd: directory stack empty ./install_uclinux: line 75: popd: directory stack empty --2014-01-11 10:23:24-- https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Attachments/8506/uboot_kernel_romfs.zip Resolving my.st.com (my.st.com)... 164.130.1.9 Connecting to my.st.com (my.st.com)|164.130.1.9|:443... connected. HTTP request sent, awaiting response... 200 OK Length: 1065782 (1.0M) [application/x-zip-compressed] Server file no newer than local file `uboot_kernel_romfs.zip' -- not retrieving. updating: install_libusbx (deflated 40%) updating: install_packages (deflated 29%) updating: install_stlink (deflated 57%) updating: install_tools (deflated 35%) updating: install_uclinux (deflated 51%) updating: flash_uclinux (deflated 60%) updating: setvars (deflated 32%) updating: readme.txt (deflated 55%) PATH:[/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/home/dzairo/uCLinux/arm-2010q1/bin:/home/dzairo/uCLinux/u-boot/tools:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games] ST-LINK flash checking to see if we linked libusbx in /usr/local/lib ldd: missing file arguments Try `ldd --help' for more information. ====== arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit ERROR arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit u-boot/stm32429-disco/u-boot.bin is missing run install_uclinux and try again ====== arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit ERROR arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit uclinux/arch/arm/boot/xipuImage.bin is missing run install_uclinux and try again ====== arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit ERROR arm-2010q1-189-arm-uclinuxeabi-i686-pc-linux-gnu.tar.bz2 build_uclinux.zip flash_uclinux install_libusbx install_packages install_stlink install_tools install_uclinux readme.txt setvars uboot_kernel_romfs.zip zipit stm32-bins/romfs.bin is missing run install_uclinux and try again dzairo@dzairo-VirtualBox:~/uCLinux$9. here I stop and no continue..
what is problem .. step by step.. I wand solve this problem.. best regards Dzairo2014-01-11 8:51 AM
root privileges required
Did you notice this line ? When installing Linux, either for ''real'' or in a VM box, you define a root password. Try using it here.
2014-01-12 11:27 PM
Hi.
I try run all scripts but still have some problem.. then :Is possible some one to run all scripts in PC and record all output in terminal to file .. and send to me ?? then I can compare with our output .. and more easy to solve problem.. is possible to do it ?? best regards.2014-01-13 7:43 PM
Hi tmk,
Can we use usb wifi on stm32f429-discovery? It is working on LPC1788 under uClinux Best regards, THANH NHI2014-01-14 10:02 AM
Hi,
the kernel doesn't contain USB HCI drivers for STM32 rightnow. I couldn't find any time to add this driver :(2014-01-16 4:34 AM
Hi. Then try use driver for SD card only .. if you have driver.. I know .. in dev kit is not sd card slot .. but this is easy to add this by wire to connect.. and make uClinux distribution with SD card support .. external drive ..and make some small program to run from SD card (mount automatic if GPIO pin is toggle to GND) .. and is possible to create file in internal FLASH ?? copy file form external SD card to internal flash.. this will possible to run program with no SD card inserted.. and start automatic..
best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.