2020-03-07 4:27 PM
Hello all,
I am very new to the STM32 environment and am just getting started with some of the basic things with the platform.
I am trying to simply read a byte of transfer from the computer on the STM32 using UART. I have enabled the interrupts and am trying to mess with the
void USART2_IRQHandler(void)The issue is that I have no clue how to access a buffer after a receive event has completed. I suppose we are expected to pass the address of a buffer variable to let the pointer transfer the data based on what I found written in stm32f4xx_hal_uart.c file. I am using the HAL drivers for this. And therefore I am doing the following,
extern UART_HandleTypeDef huart2;
uint8_t buffer;
void USART2_IRQHandler(void)
{
/* USER CODE BEGIN USART2_IRQn 0 */
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_6);
huart2.pRxBuffPtr = &buffer; //passing the buffer's address as a parameter to the pointer Not sure if this is right :\
if((buffer == 't')||(buffer == 'T'))
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_8);
__HAL_UART_CLEAR_FLAG(&huart2, UART_FLAG_TC);
__HAL_UART_CLEAR_FLAG(&huart2, UART_FLAG_RXNE);
/* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
/* USER CODE END USART2_IRQn 1 */
}The idea is to read the buffer and toggle a GPIO if character "t" is read.
Also, my UART initialization is as follows:
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
__HAL_UART_ENABLE_IT(&huart2, UART_IT_TC);
__HAL_UART_ENABLE_IT(&huart2, UART_IT_RXNE);
/* USER CODE END USART2_Init 2 */
}Any help with the resolution of this will be greatly appreciated.
Thanks in advance!
2020-03-08 3:20 AM
Hello,
If I understood correctly, you're receiving a byte from your computer and you want it to be stored in the variable 'buffer' right?
For that, you should do:
buffer = huart2.Instance->DR;
In general, your code in not optimal and might only work for 1 character
And I don't know why you're clearing the RXNE flag and TC flag
Also, I don't think you should enable UART_IT_TC flag in Init (not sure tho)
Tell me if it still doesn't work
2020-03-08 8:08 AM
Before tweaking the interrupt handler, read the HAL source and understand what it does to receive.
(Some say that reading the HAL sources is a pain .... maybe they have a point).
The HAL interrupt handler is too complex because it covers all possible cases that are not relevant or you, for example 8/9 bit units or FIFO modes.
Try to write your own small and efficient handler.
Consider the low level (LL) API instead of HAL, thru the USART2 structure - but then, maybe consider accessing the registers directly,
Decent knowledge of C is absolutely required.
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.