2024-04-17 7:48 AM - last edited on 2024-04-17 7:56 AM by mƎALLEm
Hi all,
I'm truying to adapt one file coming fromm stm32f4 discovery board for using UART. But when I try to add it to my STM NUCLEO L452RE board I got an error :
../Drivers/BSP/uart.c:328:63: error: 'USART_TypeDef' has no member named 'DR'; did you mean 'RDR'?
328 | data = (uint8_t) ((uint16_t) (s_uart1Handle.Instance->DR & (uint16_t) 0x01FF) & (uint16_t) 0x00FF);
| ^~
| RDR
Here is the function :
void USART1_IRQHandler(void)
{
uint8_t data;
uint16_t usedCapacityOfBuffer = 0;
uint16_t realCountPutBuffer = 0;
if (__HAL_UART_GET_IT_SOURCE(&s_uart1Handle, UART_IT_RXNE) != RESET &&
__HAL_UART_GET_FLAG(&s_uart1Handle, UART_FLAG_RXNE) != RESET) {
data = (uint8_t) ((uint16_t) (s_uart1Handle.Instance->DR & (uint16_t) 0x01FF) & (uint16_t) 0x00FF);
realCountPutBuffer = RingBuf_Put(&s_uart1ReadRingBuffer, &data, 1);
usedCapacityOfBuffer = UART1_READ_BUF_SIZE - RingBuf_GetUnusedSize(&s_uart1ReadRingBuffer);
s_uart1ReadBufferState.maxUsedCapacityOfBuffer =
usedCapacityOfBuffer > s_uart1ReadBufferState.maxUsedCapacityOfBuffer ? usedCapacityOfBuffer
: s_uart1ReadBufferState.maxUsedCapacityOfBuffer;
s_uart1ReadBufferState.countOfLostData += 1 - realCountPutBuffer;
}
if (__HAL_UART_GET_IT_SOURCE(&s_uart1Handle, UART_IT_TXE) != RESET &&
__HAL_UART_GET_FLAG(&s_uart1Handle, UART_FLAG_TXE) != RESET) {
if (RingBuf_Get(&s_uart1WriteRingBuffer, &data, 1)) {
/* Transmit Data */
s_uart1Handle.Instance->DR = ((uint16_t) data & (uint16_t) 0x01FF);
} else {
__HAL_UART_DISABLE_IT(&s_uart1Handle, UART_IT_TXE);
}
}
}
Do you think I can change DR by RDR? What is the difference, I've lookin for but I don't find good explaination...
Should I used TDR for transmit and RDR for receive maybe ?
Thanks
2024-04-17 7:53 AM - edited 2024-04-17 7:54 AM
@SBaro.11 wrote:Do you think I can change DR by RDR? What is the difference,
Look at the two different definitions of the USART_TypeDef structure for the two different processors (L4 and F4).
Also look at the register definitions (in the Reference Manuals) for the two processors (L4 and F4).
That should tell you if they're compatible ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.