2024-04-21 10:14 PM
Hi everyone,
I'm working on a project where I need to interface a graphic LCD with an STM32L031K6 microcontroller. I have available GPIO pins are :- PA4, PA5, PA7, PA8, PB0, PB1, PB6, PB7, PA11, PA12, PB4, and PB5.
I'm trying to print data on the LCD using the provided graphic_lcd.c and graphic_lcd.h files, along with font5x8.h. Could someone guide me on how to properly configure these GPIO pins and utilize the provided files to achieve this task?
Any insights or code snippets would be greatly appreciated. Thanks in advance for your help!
2024-10-16 8:03 AM
Hello @vinaytiwary,
You can refer to our example provided under the L0 Firmware Package:
I hope this helps you.
Otherwise, could you please provide me with more details on the main.c file, so that I can assist you further?
Thanks for your contribution.
Dor_RH
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.