2018-04-12 3:30 AM
Is there a error in theSTM32_TouchSensing_LibraryV2.1.1 with the maximum channel count for theSTM32L152ZE controller.
According to theUM1913 usermanual the STM32L1xx supports up to 34 channels.
STM32L1 series microcontrollers
– Surface charge-transfer acquisition principle managed by: – Two timers + routing interface (hardware acquisition mode). This mode is not supported on STM32L1 series microcontrollers featuring 256 K or less memory. – GPIOs + routing interface (software acquisition mode). This mode is supported by all microcontrollers. – Up to 34 channels – Up to 11 channels can be acquired simultaneouslyBut if you generate a new project with CubeMX the 'tsl_check_config_stm32l1xx.h' file has the following error checking functionality.
#if ((TSLPRM_TOTAL_CHANNELS < 1) || (TSLPRM_TOTAL_CHANNELS > 24))
#error 'TSLPRM_TOTAL_CHANNELS is out of range (1 .. 24).'
#endif
#if ((TSLPRM_TOTAL_BANKS < 1) || (TSLPRM_TOTAL_BANKS > 8))
#error 'TSLPRM_TOTAL_BANKS is out of range (1 .. 8).'
#endif
�?�?�?�?�?�?�?
these channel count does not comply with the uermanual or the datasheet of the controller.
How can I sample more then 24 channels?
I use Stm32CubeMX V4.0
STM32Cube FW_L1 V1.8.1
#cubemx-v4.0 #stm32l152We’re moving the ST Community to a new platform to give you a better and more reliable community experience.