2017-10-03 1:14 PM
I combined the code from STM32F746 discovery Template and ADC code from Cube for 746 Discovery. Something is missing allthough I checked the code several times. I use ADC3 input 6 because it is connected to a pin of Discovery board.
#include 'main.h'
#include <stdio.h>
#include 'stm32f7xx_hal.h'
#include 'stm32746g_discovery.h'
#include 'stm32746g_discovery_lcd.h'
#include <stdio.h>
#include <string.h>
#include <limits.h>
//#include 'stm32f7xx_hal.h'
#include <stdlib.h>
#include 'stm32746g_discovery_ts.h'
/** @addtogroup STM32F7xx_HAL_Examples
* @{
*/
/** @addtogroup Templates
* @{
*/
#include 'stm32746g_discovery_lcd.h'
#define LCD_FRAME_BUFFER SDRAM_DEVICE_ADDR
#define RGB565_BYTE_PER_PIXEL 2
#define ARBG8888_BYTE_PER_PIXEL 4
double ccc,kkk;
TS_StateTypeDef TS_State;
DMA2D_HandleTypeDef hdma2d;
I2C_HandleTypeDef hi2c3;
LTDC_HandleTypeDef hltdc;
UART_HandleTypeDef huart1;
DMA_HandleTypeDef hdma_memtomem_dma2_stream0;
SDRAM_HandleTypeDef hsdram1;
ADC_HandleTypeDef hadc1;
UART_HandleTypeDef huart2;
char klaa[40];
unsigned char plaa[40];
volatile int pufkuri[1];
volatile char isopuf[10];
int c,kokon;
volatile int maara;
double ccc,kkk;
static void SystemClock_Config(void);
static void Error_Handler(void);
static void MPU_Config(void);
static void CPU_CACHE_Enable(void);
/* Private functions ---------------------------------------------------------*/
static void MX_ADC1_Init(void);
int main(void)
{
uint8_t ggg;
uint8_t buf=0;
char texk[33];
uint16_t x=0, y=0;
uint8_t str[4]={0,};
MPU_Config();
/* Enable the CPU Cache */
CPU_CACHE_Enable();
HAL_Init();
/* Configure the System clock to have a frequency of 216 MHz */
SystemClock_Config();
MX_ADC1_Init();
BSP_LCD_Init();
BSP_LCD_LayerDefaultInit(LTDC_ACTIVE_LAYER, LCD_FRAME_BUFFER);
BSP_LCD_SetLayerVisible(LTDC_ACTIVE_LAYER, ENABLE);
BSP_LCD_SelectLayer(LTDC_ACTIVE_LAYER);
BSP_LCD_Clear(LCD_COLOR_BLACK);
BSP_LCD_SetBackColor(LCD_COLOR_BLACK);
BSP_LCD_SetTextColor(LCD_COLOR_WHITE);
BSP_LCD_DisplayOn();
char buffer[30] ;
sprintf(buffer,'hghhhh') ;
BSP_LCD_DisplayStringAtLine(0, (uint8_t *) buffer) ;
while (1)
{
HAL_ADC_Start(&hadc1);
if (HAL_ADC_PollForConversion(&hadc1, 1000) == HAL_OK)
{
kokon = HAL_ADC_GetValue(&hadc1);
}
HAL_ADC_Stop(&hadc1);
sprintf (klaa,'Readout %d', kokon);
BSP_LCD_DisplayStringAtLine(5, (uint8_t *) klaa) ;
}
}
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC3;
//hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = 1;
//sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief System Clock Configuration
* @param None
* @retval None
*/
static void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_OFF;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 432;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 9;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/* activate the OverDrive to reach the 216 Mhz Frequency */
if(HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief This function is executed in case of error occurrence.
* @param None
* @retval None
*/
static void Error_Handler(void)
{
/* User may add here some code to deal with this error */
while(1)
{
// BSP_LCD_DisplayStringAtLine(6, (uint8_t *) buffer) ;
}
}
static void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disable the MPU */
HAL_MPU_Disable();
/* Configure the MPU attributes as WT for SRAM */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x20010000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
static void CPU_CACHE_Enable(void)
{
/* Enable I-Cache */
SCB_EnableICache();
/* Enable D-Cache */
SCB_EnableDCache();
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line)
{
while (1)
{
}
}
#endif
/**
* @}
*/
/**
* @}
*/
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#hal_adc_pollforconversion
Solved! Go to Solution.
2017-10-03 2:37 PM
>>Something is missing although I checked the code several times
Like code to enable the ADC3 clock?
No code presented enables the pin, clocks, etc. try looking at that code.
__HAL_RCC_ADC3_CLK_ENABLE();
Polling using ADC3
STM32Cube_FW_F7_V1.8.0\Projects\STM32756G_EVAL\Examples\ADC\ADC_RegularConversion_Polling\Src\main.c
2017-10-03 2:37 PM
>>Something is missing although I checked the code several times
Like code to enable the ADC3 clock?
No code presented enables the pin, clocks, etc. try looking at that code.
__HAL_RCC_ADC3_CLK_ENABLE();
Polling using ADC3
STM32Cube_FW_F7_V1.8.0\Projects\STM32756G_EVAL\Examples\ADC\ADC_RegularConversion_Polling\Src\main.c
2017-10-05 4:12 PM
Thanks.
I checked '...\Projects\STM32756G_EVAL\Examples\ADC\ADC_RegularConversion_Polling\Src\main.c' and corrected all differencies I could find but I still get time outs. It could be that I don't use my Keil IDE optimally but finding differencies is either tedious or hit and mostly miss. There are quite a lot of .c and .h files.
2017-10-06 8:05 AM
I cant understand where are all the .c and .h files in a project. And what is changed for just current project and what not.
But I got ADC working , I think. At least there are no time outs. After a hint from Clive1 I compared files or 'mess' from an other project to my mess of files and finally got rid of time outs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.