2023-01-03 2:24 AM
Could someone assist and clarify how to configure GPDMA for DAC for use the callback function HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef* hdac) with STM32U575CGU6.
I caught:
/* Data Transfer Error Interrupt management */
if ((__HAL_DMA_GET_FLAG(hdma, DMA_FLAG_DTE) != 0U))
/* Update the DMA channel error code */
hdma->ErrorCode |= HAL_DMA_ERROR_DTE;
My goal is to catch the callback functions:
HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef* hdac) and HAL_DAC_ConvHalfCpltCallbackCh1(DAC_HandleTypeDef* hdac)
and integrate mp3 player with STM32U575CGU6.
Before STM32U575CGU6 I worked with STM32F413 and my the code worked.
Please assist.
Thanks!
Please see some parts of the code for explaining.
//////////////////////////////////////////////////////////this is a configuration of DMA //////////////
/* Includes ------------------------------------------------------------------*/
#include "gpdma.h"
/* GPDMA1 init function */
void MX_GPDMA1_Init(void)
{
/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();
/* GPDMA1 interrupt Init */
HAL_NVIC_SetPriority(GPDMA1_Channel10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(GPDMA1_Channel10_IRQn)
}
////////////////////////////////////////////////////////
//////////////////////////////////////////////////////this is configuration of DAC//////////////
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "dac.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
DAC_HandleTypeDef hdac1;
DMA_HandleTypeDef handle_GPDMA1_Channel10;
/* DAC1 init function */
void MX_DAC1_Init(void)
{
DAC_ChannelConfTypeDef sConfig = {0};
DAC_AutonomousModeConfTypeDef sAutonomousMode = {0};
/** DAC Initialization
*/
hdac1.Instance = DAC1;
if (HAL_DAC_Init(&hdac1) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT1 config
*/
sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_ABOVE_80MHZ;
sConfig.DAC_DMADoubleDataMode = DISABLE;
sConfig.DAC_SignedFormat = DISABLE;
sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
sConfig.DAC_Trigger = DAC_TRIGGER_T2_TRGO;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/** Configure Autonomous Mode
*/
sAutonomousMode.AutonomousModeState = DAC_AUTONOMOUS_MODE_DISABLE;
if (HAL_DACEx_SetConfigAutonomousMode(&hdac1, &sAutonomousMode) != HAL_OK)
{
Error_Handler();
}
}
void HAL_DAC_MspInit(DAC_HandleTypeDef* dacHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(dacHandle->Instance==DAC1)
{
/* USER CODE BEGIN DAC1_MspInit 0 */
/* USER CODE END DAC1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADCDAC|RCC_PERIPHCLK_DAC1;
PeriphClkInit.AdcDacClockSelection = RCC_ADCDACCLKSOURCE_HSI;
PeriphClkInit.Dac1ClockSelection = RCC_DAC1CLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* DAC1 clock enable */
__HAL_RCC_DAC1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**DAC1 GPIO Configuration
PA4 ------> DAC1_OUT1
*/
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* DAC1 DMA Init */
/* GPDMA1_REQUEST_DAC1_CH1 Init */
handle_GPDMA1_Channel10.Instance = GPDMA1_Channel10;
handle_GPDMA1_Channel10.Init.Request = GPDMA1_REQUEST_DAC1_CH1;
handle_GPDMA1_Channel10.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
handle_GPDMA1_Channel10.Init.Direction = DMA_MEMORY_TO_PERIPH;
handle_GPDMA1_Channel10.Init.SrcInc = DMA_SINC_INCREMENTED;
handle_GPDMA1_Channel10.Init.DestInc = DMA_DINC_FIXED;
handle_GPDMA1_Channel10.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
handle_GPDMA1_Channel10.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
handle_GPDMA1_Channel10.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel10.Init.SrcBurstLength = 1;
handle_GPDMA1_Channel10.Init.DestBurstLength = 1;
handle_GPDMA1_Channel10.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT1|DMA_DEST_ALLOCATED_PORT0;
handle_GPDMA1_Channel10.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel10.Init.Mode = DMA_NORMAL;
if (HAL_DMA_Init(&handle_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
/**DAC1 GPIO Configuration
PA4 ------> DAC1_OUT1
*/
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_4);
///////////////////////////////////////////
//////////////////////////////////////////////////////this is configuration of the timers //////////////
TIM_HandleTypeDef htim2;
/* TIM2 init function */
void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 2999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
if(tim_baseHandle->Instance==TIM2)
{
/* USER CODE BEGIN TIM2_MspInit 0 */
/* USER CODE END TIM2_MspInit 0 */
/* TIM2 clock enable */
__HAL_RCC_TIM2_CLK_ENABLE();
/* TIM2 interrupt Init */
HAL_NVIC_SetPriority(TIM2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
/* USER CODE BEGIN TIM2_MspInit 1 */
/* USER CODE END TIM2_MspInit 1 */
}
}
void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle)
{
if(tim_baseHandle->Instance==TIM2)
{
/* USER CODE BEGIN TIM2_MspDeInit 0 */
/* USER CODE END TIM2_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_TIM2_CLK_DISABLE();
/* TIM2 interrupt Deinit */
HAL_NVIC_DisableIRQ(TIM2_IRQn);
/* USER CODE BEGIN TIM2_MspDeInit 1 */
/* USER CODE END TIM2_MspDeInit 1 */
}
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
///////////////////////////////////////////
Solved! Go to Solution.
2023-01-23 11:17 PM
Hello Mohamed Aymen HZAMI (ST Employee),
Yes.
The issue was with HAL drivers (stm32u5xx_hal_dac.c).
In the file stm32u5xx_hal_dac.c on line number 869 we have function HAL_delay(1);
We need excepting HAL_delay(1) from the code and callbacks start working and SysTick_Handler() isn't stuck.
I think it's a bug of the drivers and developers will fix it.
**********************************************************************
**********************************************************************
/* Process Unlocked */
__HAL_UNLOCK(hdac);
if (status == HAL_OK)
{
/* Enable the Peripheral */
__HAL_DAC_ENABLE(hdac, Channel);
/* Ensure minimum wait before using peripheral after enabling it */
HAL_Delay(1);
}
else
{
hdac->ErrorCode |= HAL_DAC_ERROR_DMA;
}
/* Return function status */
return status;
}
**************************************************************
**************************************************************
2023-01-18 7:32 AM
Hello @Pavel D and welcome to the community,
Did you activated the DAC interruption?
Mohamed Aymen
2023-01-23 11:17 PM
Hello Mohamed Aymen HZAMI (ST Employee),
Yes.
The issue was with HAL drivers (stm32u5xx_hal_dac.c).
In the file stm32u5xx_hal_dac.c on line number 869 we have function HAL_delay(1);
We need excepting HAL_delay(1) from the code and callbacks start working and SysTick_Handler() isn't stuck.
I think it's a bug of the drivers and developers will fix it.
**********************************************************************
**********************************************************************
/* Process Unlocked */
__HAL_UNLOCK(hdac);
if (status == HAL_OK)
{
/* Enable the Peripheral */
__HAL_DAC_ENABLE(hdac, Channel);
/* Ensure minimum wait before using peripheral after enabling it */
HAL_Delay(1);
}
else
{
hdac->ErrorCode |= HAL_DAC_ERROR_DMA;
}
/* Return function status */
return status;
}
**************************************************************
**************************************************************
2023-01-24 6:02 AM
Or replace HAL_Delay(1); by function _NOP();
2023-01-30 2:32 AM
Hello @Pavel D,
Can you please share with us your project ?
Mohamed Aymen
2023-02-08 12:25 AM
2023-02-24 7:19 AM
Hello,
I can't run your project on my end, is there a specific setup you've done or could you send me a working version?
Mohamed Aymen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.