2020-09-10 11:58 PM
Hi everybody,
I have a weird problem with my STM32F302CC;In my project, HSE can work properly without USB is configured. But when I configure USB, things get weird.In debug mode, the program crash in SystemClock_Config() function when it reaches to ;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}Console shows "Target is not responding, retrying..."
As I mentioned before, with the same clock settings and USB unconfigured, the program can work properly but when I configured the USB device it starts to crash.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.