2017-09-12 4:46 PM
Hi , I'm new to STM23 and I'm currently trying to setup Ethernet communication on the NUCLEO F767ZI. Cube Mx provides great guidance but I can't seem to find any information on how to configure the initial ETH_HandleTypeDef structure in my Ethernet setup code . Is there any documentation or working example available that I can use to figure this out ?
#ethernet #nucleo-f767ziSolved! Go to Solution.
2017-09-12 6:16 PM
I used the Oryx TCP folder only, part of CycloneTCP Open.
in stm32f7xx_hal_eth.h
/**
* @brief ETH Handle Structure definition
*/
typedef struct
{
ETH_TypeDef *Instance; /*!< Register base address */
ETH_InitTypeDef Init; /*!< Ethernet Init Configuration */
uint32_t LinkStatus; /*!< Ethernet link status */
ETH_DMADescTypeDef *RxDesc; /*!< Rx descriptor to Get */
ETH_DMADescTypeDef *TxDesc; /*!< Tx descriptor to Set */
ETH_DMARxFrameInfos RxFrameInfos; /*!< last Rx frame infos */
__IO HAL_ETH_StateTypeDef State; /*!< ETH communication state */
HAL_LockTypeDef Lock; /*!< ETH Lock */
} ETH_HandleTypeDef;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
in stm32f7xx_it.c
///**
//* @brief This function handles Ethernet global interrupt.
//*/
//void ETH_IRQHandler(void)
//{
// /* USER CODE BEGIN ETH_IRQn 0 */
////////////////////
// /* USER CODE END ETH_IRQn 0 */
// HAL_ETH_IRQHandler(&heth);
// /* USER CODE BEGIN ETH_IRQn 1 */
////////////////////
// /* USER CODE END ETH_IRQn 1 */
//}�?�?�?�?�?�?�?�?�?�?�?�?�?
in main.c
extern ETH_HandleTypeDef heth;
/* ETH init function */
static void MX_ETH_Init(void)
{
uint8_t MACAddr[6] ;
heth.Instance = ETH;
heth.Init.AutoNegotiation = ETH_AUTONEGOTIATION_DISABLE;
heth.Init.Speed = ETH_SPEED_100M;
heth.Init.DuplexMode = ETH_MODE_FULLDUPLEX;
heth.Init.PhyAddress = PHY_USER_NAME_PHY_ADDRESS;
MACAddr[0] = 0x02;
MACAddr[1] = 0x80;
MACAddr[2] = 0xE1;
MACAddr[3] = 0x12;
MACAddr[4] = 0x65;
MACAddr[5] = 0x98;
heth.Init.MACAddr = &MACAddr[0];
heth.Init.RxMode = ETH_RXINTERRUPT_MODE;
heth.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE;
heth.Init.MediaInterface = ETH_MEDIA_INTERFACE_MII;
/* USER CODE BEGIN MACADDRESS */
/* USER CODE END MACADDRESS */
if (HAL_ETH_Init(&heth) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
in stm32f7xx_eth.c
/**
* @brief STM32F746/756 Ethernet MAC interrupt service routine
**/
void ETH_IRQHandler(void)
{
bool_t flag;
uint32_t status;
//Enter interrupt service routine
osEnterIsr();
//This flag will be set if a higher priority task must be woken
flag = FALSE;
//Read DMA status register
status = ETH->DMASR;
//A packet has been transmitted?
if(status & ETH_DMASR_TS)
{
//Clear TS interrupt flag
ETH->DMASR = ETH_DMASR_TS;
//Check whether the TX buffer is available for writing
if(!(txCurDmaDesc->tdes0 & ETH_TDES0_OWN))
{
//Notify the TCP/IP stack that the transmitter is ready to send
flag |= osSetEventFromIsr(&nicDriverInterface->nicTxEvent);
}
}
//A packet has been received?
if(status & ETH_DMASR_RS)
{
//Disable RIE interrupt
ETH->DMAIER &= ~ETH_DMAIER_RIE;
//Set event flag
nicDriverInterface->nicEvent = TRUE;
//Notify the TCP/IP stack of the event
flag |= osSetEventFromIsr(&netEvent);
}
//Clear NIS interrupt flag
ETH->DMASR = ETH_DMASR_NIS;
//Leave interrupt service routine
osExitIsr(flag);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
initialization in main::
int main(void)
{
/* USER CODE BEGIN 1 */
//Initialize kernel
osInitKernel();
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_TIM4_Init();
//MX_ETH_Init();
MX_DAC_Init();
MX_TIM7_Init();
/* USER CODE BEGIN 2 */
InitProcessor();
Clear_ETH_nReset_Pin();
wait_ms(1);
Set_ETH_nReset_Pin();
wait_ms(1);
MX_ETH_Init();
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2017-09-12 6:16 PM
I used the Oryx TCP folder only, part of CycloneTCP Open.
in stm32f7xx_hal_eth.h
/**
* @brief ETH Handle Structure definition
*/
typedef struct
{
ETH_TypeDef *Instance; /*!< Register base address */
ETH_InitTypeDef Init; /*!< Ethernet Init Configuration */
uint32_t LinkStatus; /*!< Ethernet link status */
ETH_DMADescTypeDef *RxDesc; /*!< Rx descriptor to Get */
ETH_DMADescTypeDef *TxDesc; /*!< Tx descriptor to Set */
ETH_DMARxFrameInfos RxFrameInfos; /*!< last Rx frame infos */
__IO HAL_ETH_StateTypeDef State; /*!< ETH communication state */
HAL_LockTypeDef Lock; /*!< ETH Lock */
} ETH_HandleTypeDef;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
in stm32f7xx_it.c
///**
//* @brief This function handles Ethernet global interrupt.
//*/
//void ETH_IRQHandler(void)
//{
// /* USER CODE BEGIN ETH_IRQn 0 */
////////////////////
// /* USER CODE END ETH_IRQn 0 */
// HAL_ETH_IRQHandler(&heth);
// /* USER CODE BEGIN ETH_IRQn 1 */
////////////////////
// /* USER CODE END ETH_IRQn 1 */
//}�?�?�?�?�?�?�?�?�?�?�?�?�?
in main.c
extern ETH_HandleTypeDef heth;
/* ETH init function */
static void MX_ETH_Init(void)
{
uint8_t MACAddr[6] ;
heth.Instance = ETH;
heth.Init.AutoNegotiation = ETH_AUTONEGOTIATION_DISABLE;
heth.Init.Speed = ETH_SPEED_100M;
heth.Init.DuplexMode = ETH_MODE_FULLDUPLEX;
heth.Init.PhyAddress = PHY_USER_NAME_PHY_ADDRESS;
MACAddr[0] = 0x02;
MACAddr[1] = 0x80;
MACAddr[2] = 0xE1;
MACAddr[3] = 0x12;
MACAddr[4] = 0x65;
MACAddr[5] = 0x98;
heth.Init.MACAddr = &MACAddr[0];
heth.Init.RxMode = ETH_RXINTERRUPT_MODE;
heth.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE;
heth.Init.MediaInterface = ETH_MEDIA_INTERFACE_MII;
/* USER CODE BEGIN MACADDRESS */
/* USER CODE END MACADDRESS */
if (HAL_ETH_Init(&heth) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
in stm32f7xx_eth.c
/**
* @brief STM32F746/756 Ethernet MAC interrupt service routine
**/
void ETH_IRQHandler(void)
{
bool_t flag;
uint32_t status;
//Enter interrupt service routine
osEnterIsr();
//This flag will be set if a higher priority task must be woken
flag = FALSE;
//Read DMA status register
status = ETH->DMASR;
//A packet has been transmitted?
if(status & ETH_DMASR_TS)
{
//Clear TS interrupt flag
ETH->DMASR = ETH_DMASR_TS;
//Check whether the TX buffer is available for writing
if(!(txCurDmaDesc->tdes0 & ETH_TDES0_OWN))
{
//Notify the TCP/IP stack that the transmitter is ready to send
flag |= osSetEventFromIsr(&nicDriverInterface->nicTxEvent);
}
}
//A packet has been received?
if(status & ETH_DMASR_RS)
{
//Disable RIE interrupt
ETH->DMAIER &= ~ETH_DMAIER_RIE;
//Set event flag
nicDriverInterface->nicEvent = TRUE;
//Notify the TCP/IP stack of the event
flag |= osSetEventFromIsr(&netEvent);
}
//Clear NIS interrupt flag
ETH->DMASR = ETH_DMASR_NIS;
//Leave interrupt service routine
osExitIsr(flag);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
initialization in main::
int main(void)
{
/* USER CODE BEGIN 1 */
//Initialize kernel
osInitKernel();
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_TIM4_Init();
//MX_ETH_Init();
MX_DAC_Init();
MX_TIM7_Init();
/* USER CODE BEGIN 2 */
InitProcessor();
Clear_ETH_nReset_Pin();
wait_ms(1);
Set_ETH_nReset_Pin();
wait_ms(1);
MX_ETH_Init();
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.