2020-10-30 11:48 PM
Hi,
We are designing the Android accessory and we would like to use STUSB4761 in our application.
STUSB4761 can source power and become device by receiving DR_swap from the sinking device.
Also we would like to put our accessory to continues in device and source to power the android phone than we can use this chip ?
In STUSB4761 there are two pins opto drv and FB that will work if I will connect 5V input
( using required components )coming from the adapter ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.