2024-08-22 4:00 AM - edited 2024-08-22 4:00 AM
Hi,
I recently purchased a STM32U5G9J -dk board. When I power up the board, TouchGFX demo application is running.
Can you please provide the source code of this demo application.
2024-08-22 6:29 AM - edited 2024-08-22 6:38 AM
Hello @PM.5
I have reported this request internally. Internal ticket number: 189199 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution
2025-05-28 3:17 AM
Hello @PM.5 ,
In TouchGFX Designer, we offer an example that closely resembles the demo application on the STM32U5G9J-DK board. This demo is named "TouchGFX Demo 6" and can be found within the TouchGFX Designer. This tool is available as a standalone software application, making it easy and quick to evaluate graphics and develop proof-of-concept projects. It is included in the X-Cube-TouchGFX package, which you can download from the following link: TouchGFX Designer.
Br
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.