STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 with FatFS on eMMC sometimes failing

Hello everyone,I have a project using the STM32H7, using FreeRTOS and with a FatFS (ChaN) runnin on a 4GB eMMC (Kingston), using peripheral SDMMC1.Normally everything works fine. SDMMC1 and FatFS (FAT32) are initialized at main, before OS, and is use...

TVare.1 by Associate III
  • 16033 Views
  • 24 replies
  • 0 kudos

Resolved! STM32U5 - USB and FreeRTOS?

I'm starting a project on the STM32U5G9, and one feature we want is USB connectivity, just a simple virtual COM port (CDC class).  Looking at the Middleware picker in CubeMX, the only USB-related items are USBPD (don't need Power Delivery at the mome...

dmarks-ls by Associate III
  • 6790 Views
  • 12 replies
  • 9 kudos

processor goes to HardFault at __ISB

Hello, I've bought Riverdi board and I'm developing a code that uses Ethernet and act as TCP server.   The code sends "Hello word %d", i++ every 10ms on that TCP socket and it works fine,   but when I try to send some byte on client size it goes to H...

MauFanGilaMedical_0-1747125665262.png

STM32N6 TCP Protocol

Does STM32N6570-DK support TCP protocol? I want to create TCP server on the board and send/receive data over 1Gbit Ethernet. How can ı do that? I didn't see the NetXDUO Protocols under NETX Middleware. It seems like it is not configurable to open UDP...

Resolved! STM32F746 Disco not debugging on W25Q128

Hello, today I received a stm32f746-disco board and I immediately coded with the external flash memory that I used on my stm32f750-disco, the problem is that the code doesn't work and I can't debug (before this was easy to do on the f750), after test...

OWLchan by Associate III
  • 2139 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.