2023-03-26 7:07 AM
We are not sure it really jumps to the bootloader
Please see code attached, especially note if required to add code for memory remapping:
void jump_to_bootloader(void) {
void (*SysMemBootJump)(void);
/**
* Step: Set system memory address.
*
* For STM32U575xx, system memory is at 0x0BF90000
* For other families, check AN2606 document
*/
volatile uint32_t addr = 0x0BF90000; // STM32U575xx
/**
* Step: Disable RCC, set it to default (after reset) settings
* Internal clock, no PLL, etc.
*/
HAL_RCC_DeInit();
/**
* Step: Disable systick timer and reset it to default values
*/
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
/**
* Step: Disable all interrupts
*/
__disable_irq();
// /**
// * Step: Remap system memory to address 0x0000 0000 in address space
// * For each family registers may be different.
// * Check reference manual for each family.
// *
// * For STM32F4xx, MEMRMP register in SYSCFG is used (bits[1:0])
// * For STM32F0xx, CFGR1 register in SYSCFG is used (bits[1:0])
// * For others, check family reference manual
// */
// //Remap by hand... {
// SYSCFG->MEMRMP = 0x01; //F7
/**
* Step: Set jump memory location for system memory
* Use address with 4 bytes offset which specifies jump location where program starts
*/
SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
/**
* Step: Set main stack pointer.
* This step must be done last otherwise local variables in this function
* don't have proper value since stack pointer is located on different position
*
* Set direct address location which specifies stack pointer in SRAM location
*/
__set_MSP(*(uint32_t *)addr);
/**
* Step: Actually call our function to jump to set location
* This will start system memory execution
*/
SysMemBootJump();
/**
* Step: Connect USB<->UART converter to dedicated USART pins and test
* and test with bootloader works with STM32 Flash Loader Demonstrator software
*/
}
2023-03-26 7:33 AM
>>We are not sure it really jumps to the bootloader
Step the transition with the debugger
>>__disable_irq(); // Step: Disable all interrupts
Not the means to the end. You really want to disable the interrupt you have enabled at the peripherals. Not disable IRQs entirely on the MCU. Nothing on the other side reenables them, they are not disabled at startup normally.
2023-03-26 7:47 AM
Thank you for your answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.