2023-12-04 8:27 PM
We use STM32CubeMX and STM32U5. STM32U5 supports linked list DMA transfers. But HAL_ADC_Start_DMA() will not do a transfer larger than 64k. It only creates the first element in the list and exits. In addition, HAL_ADC_Start_DMA() doesn't give an error when Length > 64k, instead it trucates the uint32_t to 16-bits silently.
2023-12-04 11:59 PM - edited 2023-12-05 12:03 AM
you could read the rm , to see, what the dma can or not can do :
so one block transfer is max. 64K.
>it trucates the uint32_t to 16-
- the register is 16bits - so what should it do? give error message : RTFM ! :)
2023-12-05 1:28 PM
No, it should create a linked list of more than 1 transfer.
I'm complaining because my code worked on previous STM32: 52000 size, half-word(uint16_t) transfer size. Now same code no longer works and gave no error. Also I would expect the call HAL_ADC_Start_DMA() to work.
Is there another HAL call I should be using that doesn't just create one linked list entry and then "gives up"?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.