2023-04-21 7:12 AM
Hi,
I am developing a sensor board that includes an STM32U575CGTx MCU, an IMU, a microSD card slot, USB, and a battery (rough schematic attached). If you have a better suggestion for the MCU, please feel free to suggest it. The data logging rate is relatively low at 60 kB/s, and the IMU sample rate is 1600 Hz.
The basic requirements for the sensor board are as follows:
ChatGPT suggested the following steps to achieve these requirements:
I must point out that I am not highly skilled in programming, although I have completed a similar project using Arduino. This project is a step towards more professional development. Could you point me towards any examples or specific paragraphs in datasheets that may be helpful?
EDIT: more specific questions will follow as the project goes on.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.