2025-08-20 9:13 AM - last edited on 2025-08-21 12:46 AM by mƎALLEm
Hello,
I am starting a timer interrupt to send data over can data at 50 ms below is the configuration for the same and callback function when pulse is complete
volatile uint8_t send_ch0_flag = 0;
volatile uint8_t send_chx_flag = 0;
volatile uint8_t send_relay_flag = 0;
void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim2.Instance = TIM2;
htim2.Init.Prescaler = 3999; // 80 MHz / (3999+1) = 20 kHz
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 999; // (999+1) / 20kHz = 0.05 s = 50 ms
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
__HAL_RCC_TIM2_CLK_ENABLE();
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
HAL_NVIC_SetPriority(TIM2_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
HAL_TIM_Base_Start_IT(&htim2);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM2)
{
ms_counter += 50;
// Channel 0 every 50 ms
send_ch0_flag = 1;
// Channels 1–8 every 100 ms
if (ms_counter % 100 == 0) {
send_chx_flag = 1;
}
// Relay every 1000 ms
if (ms_counter % 1000 == 0) {
send_relay_flag = 1;
ms_counter = 0; // reset counter
}
}
}
void process_CAN_messages(void) //called inside while loop
{
if (send_ch0_flag) {
send_ch0_flag = 0;
CAN_SendChannel(0); // your wrapper function
}
if (send_chx_flag) {
send_chx_flag = 0;
for (int ch = 1; ch < 9; ch++) {
CAN_SendChannel(ch);
}
}
if (send_relay_flag) {
send_relay_flag = 0;
sendRelayMessages();
}
}
Please let me know what configuration I am doing wrong or is it a code issue.
But when I send a command over can to the mcu I am not able to recieve the command but the same is working when I am starting the timer at 100ms. Below is the can reception logic. The CAN transrx ic i am using is TLE9255W.
Inside while I am monitoring my can transrx interrupt below is the interrupt
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan){
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData);
if(RxHeader.DLC == 8){
data_received = 1; //monitored inside while loop
}
}
Thanks
2025-08-21 12:49 AM
Hello,
I'm not sure I understood the issue. Please elaborate more that statement:
@yashg25 wrote:
But when I send a command over can to the mcu I am not able to recieve the command but the same is working when I am starting the timer at 100ms. Below is the can reception logic. The CAN transrx ic i am using is TLE9255W.
2025-08-21 1:09 AM
Hello @mƎALLEm ,
What I meant by that statement is that :
Statement 1:
When I set the timer period to generate interrupt at every 50ms (for sending data from stm32l452re to CAN device which is working but on my CAN device I see the reception time around 90ms even for a 50ms interrupt),
I am not able to send the can command from my CAN device to stm32l452re CAN, the command is not executing.
Statement 2:
But when I set the timer period to generate interrupt at every 100ms(for sending data from stm32l452re to CAN device which is working and on my CAN device I see the reception time around 100ms),
I am able to send the can commands from my CAN device to stm32l452re CAN, the command that I am sending are executing.
Thanks,
Yash
2025-08-21 9:09 PM
@mƎALLEm , Waiting for your reply.
2025-08-25 3:30 AM
Hi @yashg25,
Since CAN communication fails when the timer interrupt is set to 50 ms but works at 100 ms, this is likely due to interrupt timing conflicts or priority mismanagement; the timer interrupt can be preempting the CAN interrupt, can you share interrupt priorities?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-26 5:26 AM
Hello @Sarra.S,
Below are the priorities :
1. Timer interrupt
HAL_NVIC_SetPriority(TIM2_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
2. CAN interrupt
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
Regards,
Yash Gupta
2025-08-26 11:47 AM
You're not showing enough code.
What is going on in CAN_SendChannel and sendRelayMessages?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.