2016-05-15 11:52 PM
Hi,
I am using STM32L4 Discovery Kit and wanted to check the DFU Programming.For that, I programmed the GPIO_IOToggle Code and then shorted the BOOT0 pin with 3V.Then pressed Reset button.But nothing happens.Can somebody please tell if anything from the Software side needs to be configured ?Thanks,Sunny #stm32l4 #dfu2016-05-16 2:19 AM
Are you using the right USB connector? ie The micro USB at the bottom not the ST-LINK one at the top.
2016-05-16 2:44 AM
Hi clive1,
I am using both the USB Connectors i.e. USB User (Micro-USB) to get detected as ST-Link Device in DFU Mode and the other i.e. USB ST-Link which will give supply to the STM32L4 Discovery Kit.The USB ST-Link Debugger is getting enumerated in the Windows Device Manager, but the micro USB port for DFU Mode is not getting enumerated.Please advice.Thanks,Sunny2016-05-17 5:44 AM
Hi Sunny,
What you are doing works for me, I can enter dfu mode on the L4disco. Maybe you micro cable is broken....2016-05-18 10:33 PM
Hi Edje,
Thanks for the pointer.I already checked with 3 different cables which are working with cellphones, but not working with the L4 Discovery Kit.Thanks,SunnyWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.