2015-02-21 10:40 AM
Hello
I just need a confirmation. Is there really no support for firmware upgrade over USB (DFU) in the STM32L0 MCUs??? The STM32L0 is not listed in the document. But in the CubeMX tool the DFU usb profile can be selected for STM32L0 MCUs. Is DFU supported or not? Thank you #stm32l0-dfu2015-02-21 3:00 PM
The 4K ROM in the L053 doesn't seem to be adequate to support USB/DFU.
Perhaps Cube referencing a FLASH based DFU loader?2016-04-05 9:30 AM
Hi fischbach.paul,
If you refer to table 3 of , you should find the information that DFU bootloader is available for STM32L07/L08 devices.Then, AN3156 will be updated to include STM32L0.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.