2024-10-17 2:12 AM - last edited on 2024-10-17 2:41 AM by mƎALLEm
I try for the first time to use audio , on my stm32h747i-DISCO board.
I have 2 questions
1) the build CM7 is showing the following error
Description Resource Path Location Type
'Mode' undeclared (first use in this function) stm32h7xx_hal_msp.c /stm32h7disco-i2s-baremetal_CM7/Core/Src line 179 C/C++ Problem
in
/* USER CODE END I2S1_Init 1 */
hi2s1.State = HAL_I2S_STATE_RESET;
hi2s1.Instance = SPI1;
hi2s1.Init.Mode = Mode;
hi2s1.Init.Standard = I2S_STANDARD_PHILIPS;
hi2s1.Init.DataFormat = I2S_DATAFORMAT_16B_EXTENDED;
hi2s1.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
hi2s1.Init.AudioFreq = I2S_AUDIOFREQ_11K;
hi2s1.Init.CPOL = I2S_CPOL_LOW;
hi2s1.Init.FirstBit = I2S_FIRSTBIT_MSB;
hi2s1.Init.WSInversion = I2S_WS_INVERSION_DISABLE;
hi2s1.Init.Data24BitAlignment = I2S_DATA_24BIT_ALIGNMENT_RIGHT;
hi2s1.Init.MasterKeepIOState = I2S_MASTER_KEEP_IO_STATE_DISABLE;
if (HAL_I2S_Init(&hi2s1, Mode) != HAL_OK) //This Mode is the error
{
Error_Handler();
}
/* USER CODE BEGIN I2S1_Init 2 */
/* USER CODE END I2S1_Init 2 */
}
Even after regenerating the code, the error is still here
I imagine the input is Jack microphone aud the output is Jack speaker.
The notice says I2S pins
- PA4: i2s1_ws
- PA6: i2s1_sdi :Digital pin5 of the arduino connector below the Disco Module.
- PB3: i2s1_ck
- PD7: i2s1_sdo I am not usual of I2S, may be the output is I2S1_SDO pin (But, I don't see any access to this pin).
Solved! Go to Solution.
2024-10-17 2:33 AM
You are probably referring to Github project of gokmez?
Have you already contacted him and asked him about it?
Regards
/Peter
2024-10-17 2:33 AM
You are probably referring to Github project of gokmez?
Have you already contacted him and asked him about it?
Regards
/Peter
2024-10-17 2:39 AM
Hello @BRobe.3 ,
@BRobe.3 wrote:
I try for the first time to use audio , on my stm32h747i-DISCO board.
Which Demo? you need always to provide details from the beginning to prevent confusions ..
Also, please use </> button to share your code. Refer to the tips on how to post a thread.
Thank you.
2024-10-17 5:33 AM
Thanks for your answer. Yes it is https://github.com/gokmez/stm32h7-i2s-record-play-wav.
I will try contact him
Best regards
2024-10-17 5:36 AM
Thanks for your answer
It is : https://github.com/gokmez/stm32h7-i2s-record-play-wav for stm32h747i-DISCO board.
Best Regards
2024-10-26 3:07 AM
Hello Peter,
Unfortunatly, I didn't find any way to contact Mr Gokmez.
Do you have a contact ? It would be great to find a solution as it is the only sound example for the stm32h7disco board.
Best Regards
2024-10-26 5:10 AM - edited 2024-10-26 5:10 AM
Gokmez is one of millions of users of the STM32 MCUs. I could also just try to reach him via GitHub, as I also only found the repository with my favourite search engine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.