2022-04-09 2:41 AM
Hi,
We are using STM32H747IG microcontroller in our custom board and have connected the USART1 pins PA9 & PA10 to the host processor to update the firmware using UART.
The USART1 pins PB14 & PB15 are connected to the LEDs using a NPN transistor and will be configured in our application a GPIO.
In the host processor we are using the stm32flash Linux utility & this utility sends 0x7F byte twice.
After making the BOOT0 pin HIGH & power cycling the board, the STM32 MCU is not responding to the USART1 pins PA9 & PA10. But the LEDs connected to PB14 & PB15 are glowing.
Later we connected the host processor UART to PB14 & PB15 by making some hardware changes in the board. After this change, the stm32flash utility successfully flashed the STM32 MCU.
We also have a Discovery kit with STM32H747XIH6U MCU & connected it's PB14 & PB15 USART1 lines available at the STMOD+ connector P2 to our host processor and shorted resistor R192 as suggested in the User Manual to change the BOOT0 pin to HIGH. We could easily flash the firmware using the stm32flash utility from our host processor.
I have the following questions regarding the USART1 pins:
Anyway we are going for the revision of our custom board in a few weeks. If we cannot use PA9 & PA10 pins for USART1 bootloader flashing then we will use PB14 & PB15 pins.
Thanks & Regards,
Pravardhan U.S
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.